<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8 UUU in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-UUU/m-p/1199257#M166459</link>
    <description>&lt;P&gt;Hi gravity&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;reason may be in versions incompatibility between RPA tool, SCFW, kernel and uuu versions.&lt;/P&gt;
&lt;P&gt;So may be suggested to rebuild all image from scratch using latest revisions of&lt;/P&gt;
&lt;P&gt;RPA tool and ddr test , SCFW and kernel as described in Release Notes document for each BSP on link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 02:40:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-12-15T02:40:40Z</dc:date>
    <item>
      <title>imx8 UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-UUU/m-p/1198952#M166433</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;modiy SCFW&amp;amp;uboot(include/config/imx8qxq_mek.h)&amp;nbsp; DDR 3GB--&amp;gt;2GB&lt;/P&gt;&lt;P&gt;use download 2GB.bin to 3GBDDR board,is ok,&amp;nbsp; uboot startup is 2GB.&lt;/P&gt;&lt;P&gt;but&amp;nbsp;download 2GB.bin to 2GBDDR board,is erro,&lt;/P&gt;&lt;LI-CODE lang="c"&gt;D:\v1_UUU&amp;gt;uuu -V -b qspi imx-boot-800-es2-c0-fspi.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.191-0-g4fe24b9

Build in config:
        Pctl     Chip            Vid     Pid     BcdVersion
        ==================================================
        SDPS:    MX8QXP          0x1fc9  0x012f  [0x0002..0xffff]
        SDPS:    MX8QM           0x1fc9  0x0129  [0x0002..0xffff]
        SDPS:    MX8DXL          0x1fc9  0x0147
        SDPS:    MX28            0x15a2  0x004f
        SDPS:    MX815           0x1fc9  0x013e
        SDPS:    MX865           0x1fc9  0x0146
        SDP:     MX7D            0x15a2  0x0076
        SDP:     MX6Q            0x15a2  0x0054
        SDP:     MX6D            0x15a2  0x0061
        SDP:     MX6SL           0x15a2  0x0063
        SDP:     MX6SX           0x15a2  0x0071
        SDP:     MX6UL           0x15a2  0x007d
        SDP:     MX6ULL          0x15a2  0x0080
        SDP:     MX6SLL          0x1fc9  0x0128
        SDP:     MX7ULP          0x1fc9  0x0126
        SDP:     MXRT106X        0x1fc9  0x0135
        SDP:     MX8MM           0x1fc9  0x0134
        SDP:     MX8MQ           0x1fc9  0x012b
        SDPU:    SPL             0x0525  0xb4a4  [0x0000..0x04ff]
        SDPV:    SPL1            0x0525  0xb4a4  [0x0500..0x9998]
        SDPU:    SPL             0x0525  0xb4a4  [0x9999..0x9999]
        SDPU:    SPL             0x3016  0x1001  [0x0000..0x04ff]
        SDPV:    SPL1            0x3016  0x1001  [0x0500..0x9998]
        FBK:                     0x066f  0x9afe
        FBK:                     0x066f  0x9bff
        FB:                      0x0525  0xa4a5
        FB:                      0x18d1  0x0d02
        FB:                      0x3016  0x0001

Run built-in script:

uuu_version 1.2.39

# &amp;lt;li-user uid="40832" login="imx"&amp;gt;&amp;lt;/li-user&amp;gt;-boot-800-es2-c0-fspi.bin            | bootloader
# &amp;lt;li-user uid="40832" login="imx"&amp;gt;&amp;lt;/li-user&amp;gt;-boot-800-es2-c0-fspi.bin   [imx-boot-800-es2-c0-fspi.bin] | image burn to flexspi, default is the same as bootloader

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-800-es2-c0-fspi.bin

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM, skip QSPI header
SDPS: boot -f imx-boot-800-es2-c0-fspi.bin -skipfhdr

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-800-es2-c0-fspi.bin -offset 0x10000 -skipfhdr
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-800-es2-c0-fspi.bin -skipspl -skipfhdr
SDPV: jump
# }

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f imx-boot-800-es2-c0-fspi.bin

# Check Image if include flexspi header
FB: ucmd if qspihdr dump ${fastboot_buffer}; then setenv qspihdr_exist yes; else setenv qspihdr_exist no; fi;

FB[-t 60000]: ucmd if test ${qspihdr_exist} = yes; then qspihdr init ${fastboot_buffer} ${fastboot_bytes} safe; else true; fi;

#if uboot can't support qspihdr command, use uboot image to write qspi image, which require image include qspi flash header
FB: ucmd if test ${qspihdr_exist} = no; then sf probe; else true; fi;
FB[-t 40000]: ucmd if test ${qspihdr_exist} = no; then sf erase 0 +${fastboot_bytes}; else true; fi;
FB[-t 20000]: ucmd if test ${qspihdr_exist} = no; then sf write ${fastboot_buffer} 0 ${fastboot_bytes}; else true; fi;
FB: done


Wait for Known USB Device Appear...
New USB Device Attached at 2:4
2:4&amp;gt;Start Cmd:SDPS: boot -f imx-boot-800-es2-c0-fspi.bin -skipfhdr
100%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 裝置沒有連線。
2:4&amp;gt;Okay (0.255s)
libusb: warning [init_device] could not get node connection information for device 'USB\VID_0E0F&amp;amp;PID_0001\5&amp;amp;1FC31FA8&amp;amp;0&amp;amp;4': [87] 參數錯誤。
New USB Device Attached at 2:4
2:4&amp;gt;Start Cmd:SDPV: delay 1000
2:4&amp;gt;Okay (1.019s)
2:4&amp;gt;Start Cmd:SDPV: write -f imx-boot-800-es2-c0-fspi.bin -skipspl -skipfhdr
100%2:4&amp;gt;Okay (1.005s)
2:4&amp;gt;Start Cmd:SDPV: jump
6400%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 裝置沒有連線。
2:4&amp;gt;Okay (0.063s)
libusb: warning [init_device] could not get node connection information for device 'USB\VID_0E0F&amp;amp;PID_0001\1817A00E828C1720': [87] 參數錯誤。
New USB Device Attached at 2:4
2:4&amp;gt;Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}
2:4&amp;gt;Okay (0.002s)
2:4&amp;gt;Start Cmd:FB: download -f imx-boot-800-es2-c0-fspi.bin
2:4&amp;gt;Okay (0.042s)
2:4&amp;gt;Start Cmd:FB: ucmd if qspihdr dump ${fastboot_buffer}; then setenv qspihdr_exist yes; else setenv qspihdr_exist no; fi;
2:4&amp;gt;Okay (0.072s)
2:4&amp;gt;Start Cmd:FB[-t 60000]: ucmd if test ${qspihdr_exist} = yes; then qspihdr init ${fastboot_buffer} ${fastboot_bytes} safe; else true; fi;
2:4&amp;gt;Okay (0.043s)
2:4&amp;gt;Start Cmd:FB: ucmd if test ${qspihdr_exist} = no; then sf probe; else true; fi;
2:4&amp;gt;Fail (0.117s)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2GB DDR stress test is ok!&lt;/P&gt;&lt;LI-CODE lang="c"&gt;*************************************************************************
       MX8 DDR Stress Test Version: ER14
       Built on Mar 27 2020 12:28:23
*************************************************************************

--Set up the MMU and enable I and D cache--
   - This is the Cortex-A35 core
  - Check if I cache is enabled 
  - Enabling I cache since it was disabled 
  - Push base address of TTB to TTBR0_EL3 
  - Config TCR_EL3 
  - Config MAIR_EL3 
  - Enable MMU 
  - Data Cache has been enabled 
  - Check system memory register, only for debug 

   - VMCR Check:
   - ttbr0_el3: 0x13d000
   - tcr_el3: 0x2051c
   - mair_el3: 0x774400
   - sctlr_el3: 0xc01815
   - id_aa64mmfr0_el1: 0x101122

  - MMU and cache setup complete 

*************************************************************************
            ARM Clock(CA35): 1200MHz
            DDR Clock: 1200MHz

============================================
        DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
One chip select is used 
Number of DDR controllers used on the SoC: 1
Density per chip select:   2048MB 
Density per controller is: 2048MB 
Total density detected on the board is: 2048MB 

No DDR data training errors detected for DDRC0
============================================

MX8QXP: Cortex-A35 is found

*************************************************************************
DDR Stress Test Iteration 1
  -------------------------------- 
  --Running DDR test on region 1-- 
  -------------------------------- 

t0.1: data is addr test
....
t0.2: row hop read test
...

t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test 
....................................................................
t4: IRAM_to_DDRv1 test
...

t5: IRAM_to_DDRv2 test

Success: DDR Stress test completed!!!&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;gravity&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 13:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-UUU/m-p/1198952#M166433</guid>
      <dc:creator>gravity_one</dc:creator>
      <dc:date>2020-12-14T13:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-UUU/m-p/1199257#M166459</link>
      <description>&lt;P&gt;Hi gravity&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;reason may be in versions incompatibility between RPA tool, SCFW, kernel and uuu versions.&lt;/P&gt;
&lt;P&gt;So may be suggested to rebuild all image from scratch using latest revisions of&lt;/P&gt;
&lt;P&gt;RPA tool and ddr test , SCFW and kernel as described in Release Notes document for each BSP on link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 02:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-UUU/m-p/1199257#M166459</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-15T02:40:40Z</dc:date>
    </item>
  </channel>
</rss>