<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Wayland does not support QWindow::requestActivate()</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-does-not-support-QWindow-requestActivate/m-p/1198974#M166435</link>
    <description>&lt;P&gt;Hello darshak,&lt;/P&gt;
&lt;P&gt;Make sure that you are using the latest BSP, Qt 5 is built into the Linux image in the Yocto Project environment with the command bitbake imx-image-full.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Dec 2020 14:20:43 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-12-14T14:20:43Z</dc:date>
    <item>
      <title>Wayland does not support QWindow::requestActivate()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-does-not-support-QWindow-requestActivate/m-p/1198141#M166350</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the past, I have implemented one qt5 app in c++ on the 4.14 sumo release, and that demo working fine.&lt;/P&gt;&lt;P&gt;Now I am using imx8mq board and 5.4 Zeus release and build the same demo and try to run but it throws below error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mqevk:~# /usr/share/chemicalplanthmi-1.0/ChemicalPlantHMI qt.qpa.wayland: Wayland does not support QWindow::requestActivate()  &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help me how can I resolve the above error?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 14:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-does-not-support-QWindow-requestActivate/m-p/1198141#M166350</guid>
      <dc:creator>darsh_dev</dc:creator>
      <dc:date>2020-12-11T14:23:22Z</dc:date>
    </item>
    <item>
      <title>Re: Wayland does not support QWindow::requestActivate()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-does-not-support-QWindow-requestActivate/m-p/1198974#M166435</link>
      <description>&lt;P&gt;Hello darshak,&lt;/P&gt;
&lt;P&gt;Make sure that you are using the latest BSP, Qt 5 is built into the Linux image in the Yocto Project environment with the command bitbake imx-image-full.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 14:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-does-not-support-QWindow-requestActivate/m-p/1198974#M166435</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-12-14T14:20:43Z</dc:date>
    </item>
  </channel>
</rss>