<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Player based on imX8MQ board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1198307#M166365</link>
    <description>&lt;P&gt;thanks,&lt;SPAN class="tgt"&gt;I have loaded the required modules into the system as you said. Based on this, I developed a player that can play videos normally, but if I frequently adjust the progress or volume of videos, the system will crash and restart.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;Please give me some instructions on how To solve this problem.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 12 Dec 2020 02:56:57 GMT</pubDate>
    <dc:creator>Joe_C</dc:creator>
    <dc:date>2020-12-12T02:56:57Z</dc:date>
    <item>
      <title>Player based on imX8MQ board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1192109#M165843</link>
      <description>&lt;P&gt;I used the yocto provided by the player in the routine, and copy it into the board, the path of the routine for "build - xwayland/TMP/work/aarch64 - poky - Linux/qtmultimedia 5.12.3 + gitAUTOINC + 64981 aee3b r0 / image/usr/share/examples/multimediawidgets/player".When playing A video, the CPU is 100% used, and the terminal prints out A Warning:A lot of buffers are being dropped.What can I do to play the video properly using this routine&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="que1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131524i3DAA2AC972C391E9/image-size/large?v=v2&amp;amp;px=999" alt="que1.png" title="que1.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 07:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1192109#M165843</guid>
      <dc:creator>Joe_C</dc:creator>
      <dc:date>2020-12-02T07:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Player based on imX8MQ board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1193664#M165968</link>
      <description>&lt;P&gt;how about adding&lt;/P&gt;
&lt;P&gt;IMAGE_INSTALL_append = "\&lt;BR /&gt;qtmultimedia \&lt;BR /&gt;qtmultimedia-plugins \&lt;BR /&gt;qtmultimedia-examples \&lt;BR /&gt;qtmultimedia-qmlplugins" to the local.conf,&amp;nbsp; and add PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer" to local.conf too, then when the board boot up, to find /usr/share/examples/multimedia/video/qmlvideo&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Dec 2020 04:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1193664#M165968</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-04T04:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: Player based on imX8MQ board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1198307#M166365</link>
      <description>&lt;P&gt;thanks,&lt;SPAN class="tgt"&gt;I have loaded the required modules into the system as you said. Based on this, I developed a player that can play videos normally, but if I frequently adjust the progress or volume of videos, the system will crash and restart.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;Please give me some instructions on how To solve this problem.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 12 Dec 2020 02:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1198307#M166365</guid>
      <dc:creator>Joe_C</dc:creator>
      <dc:date>2020-12-12T02:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: Player based on imX8MQ board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1232483#M169639</link>
      <description>&lt;P&gt;current qt multimedia only supports play video normally, if you need other feature, customer needs debug by themselves, we don't offer these, or you can find more information from QT forum to further information&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 02:51:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Player-based-on-imX8MQ-board/m-p/1232483#M169639</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-02-18T02:51:41Z</dc:date>
    </item>
  </channel>
</rss>