<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MM Android10 SD Boot failure state LOCK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198023#M166331</link>
    <description>&lt;P&gt;The controller connected to the SDcard slot is set to work with Wi-Fi expansion card in Android10.0.0_2.5.0 demo image, it does not support to access SDcard.&lt;/P&gt;
&lt;P&gt;so basically, if the dtbo image support Wi-Fi expansion card, then the images cannot boot up from SD card.&lt;/P&gt;</description>
    <pubDate>Fri, 11 Dec 2020 10:04:11 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2020-12-11T10:04:11Z</dc:date>
    <item>
      <title>IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195231#M166114</link>
      <description>&lt;P&gt;hello，I use imx8mm android10，I only modified the SD card pins，uboot-imx/arch/arm/dts/imx8mm-evk.dts：&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;369 &amp;amp;usdhc2 {&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;370&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-names = "default", "state_100mhz", "state_200mhz";&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;371&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_usdhc2&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;372&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-1 = &amp;lt;&amp;amp;pinctrl_usdhc2_100mhz&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;373&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-2 = &amp;lt;&amp;amp;pinctrl_usdhc2_200mhz&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;374&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //cd-gpios = &amp;lt;&amp;amp;gpio1 15 GPIO_ACTIVE_LOW&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;&lt;FONT color="#FF0000"&gt;375&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cd-gpios = &amp;lt;&amp;amp;gpio2 12 GPIO_ACTIVE_LOW&amp;gt;;//add cjf&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/FONT&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;376&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bus-width = &amp;lt;4&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;377&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmmc-supply = &amp;lt;&amp;amp;reg_usdhc2_vmmc&amp;gt;;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;378&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;379 };&lt;/SPAN&gt;&lt;SPAN&gt;After compiling uboot, burn the image to the SD card：sudo ./fsl-sdcard-partition.sh -f imx8mm /dev/sdb&lt;BR /&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="6$A`]78{_`(X)B6{][)$91V.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132075i52DF41C961F08412/image-size/medium?v=v2&amp;amp;px=400" role="button" title="6$A`]78{_`(X)B6{][)$91V.png" alt="6$A`]78{_`(X)B6{][)$91V.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;6$A`]78{_`(X)B6{][)$91V.png&lt;/span&gt;&lt;/span&gt;&lt;P&gt; uboot&amp;nbsp;Boot failure：&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;U-Boot 2020.04-dirty (Dec 07 2020 - 17:51:27 +0800)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 50C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;&lt;P&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 0263634&lt;BR /&gt;- U-Boot 2020.04-dirty&lt;/P&gt;&lt;P&gt;flash target is MMC:1&lt;BR /&gt;Net:&lt;BR /&gt;Error: ethernet@30be0000 address not set.&lt;/P&gt;&lt;P&gt;Error: ethernet@30be0000 address not set.&lt;BR /&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;avb_slot_verify.c:772: ERROR: vbmeta_a: Error loading vbmeta data.&lt;BR /&gt;verify FAIL, state: LOCK&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;What should I do?&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 08 Dec 2020 07:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195231#M166114</guid>
      <dc:creator>jianfeichang</dc:creator>
      <dc:date>2020-12-08T07:09:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195424#M166124</link>
      <description>&lt;P&gt;Could you tell us are you using the reference board or the board you design by yourself? And which andorid10 are you using?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 10:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195424#M166124</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-12-08T10:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195425#M166125</link>
      <description>&lt;P&gt;I used my own design board, referring to the IMX8mm EVK LPDDR4。it is android-10.0.0_2.5.0_image_8mmevk.tar.gz，Just a change in the SD card pin。&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 10:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1195425#M166125</guid>
      <dc:creator>jianfeichang</dc:creator>
      <dc:date>2020-12-08T10:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1197855#M166320</link>
      <description>&lt;P&gt;Now I have the same problem with the official image，emmc is ok，Sd card prompts lock error。android-10.0.0_2.5.0_image_8mmevk.tar.gz&amp;nbsp; imx8mm lpddr4 sd 32G EMMC16G。&lt;/P&gt;&lt;P&gt;android 9 is ok。linux 4.14.98 is ok。emmc and sd。&lt;/P&gt;&lt;P&gt;One more question：&lt;/P&gt;&lt;P&gt;Burn the image using&amp;nbsp;uuu_imx_android_flash.bat，windows7/10 and ubuntu，There will be temporary files that cannot be deleted automatically and need to be manually deleted。&amp;nbsp;C:\Users\cjf\AppData\Local\Temp ，ubuntu ls /tmp/&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 05:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1197855#M166320</guid>
      <dc:creator>jianfeichang</dc:creator>
      <dc:date>2020-12-11T05:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198023#M166331</link>
      <description>&lt;P&gt;The controller connected to the SDcard slot is set to work with Wi-Fi expansion card in Android10.0.0_2.5.0 demo image, it does not support to access SDcard.&lt;/P&gt;
&lt;P&gt;so basically, if the dtbo image support Wi-Fi expansion card, then the images cannot boot up from SD card.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:04:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198023#M166331</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-12-11T10:04:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198024#M166332</link>
      <description>&lt;P&gt;This android-10.0.0_2.3.0 version should be work. You can have a try.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:05:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198024#M166332</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-12-11T10:05:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198028#M166334</link>
      <description>&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;I want to use Android10_2.5.0，My wifi card is AP6255 BCM43455，How do I modify an &lt;SPAN&gt;dtbo image？Get rid of its own wifi card?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198028#M166334</guid>
      <dc:creator>jianfeichang</dc:creator>
      <dc:date>2020-12-11T10:14:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198030#M166335</link>
      <description>&lt;P&gt;You need to download the source and porting your wifi to your board.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198030#M166335</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-12-11T10:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198031#M166336</link>
      <description>&lt;P&gt;You can not use the demo images supply in our website, it's for the reference board.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198031#M166336</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-12-11T10:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM Android10 SD Boot failure state LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198035#M166337</link>
      <description>&lt;P&gt;Thank you. Can I remove the official wifi card？&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 10:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-Android10-SD-Boot-failure-state-LOCK/m-p/1198035#M166337</guid>
      <dc:creator>jianfeichang</dc:creator>
      <dc:date>2020-12-11T10:27:21Z</dc:date>
    </item>
  </channel>
</rss>