<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックOpenCV Packages with yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1196598#M166190</link>
    <description>&lt;P&gt;Hello I have a two part question.&lt;/P&gt;&lt;P&gt;1). I bitbaked the fsl-image-qt5-validation-imx for my IMX8M Quad and I have a Qt application that uses Opencv 4.4. This image builds opencv 4.2. How would I be able to upgrade to 4.4?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2). I also use "Qt5GstreamerUi-1.0, Qt5GstreamerUtils-1.0, gstreamer-1.0 and gstreamer1.0-app" packages in the application. What would I need to add to my local.conf in order to get these packages on the IMX8?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Dec 2020 16:07:59 GMT</pubDate>
    <dc:creator>rthomas</dc:creator>
    <dc:date>2020-12-09T16:07:59Z</dc:date>
    <item>
      <title>OpenCV Packages with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1196598#M166190</link>
      <description>&lt;P&gt;Hello I have a two part question.&lt;/P&gt;&lt;P&gt;1). I bitbaked the fsl-image-qt5-validation-imx for my IMX8M Quad and I have a Qt application that uses Opencv 4.4. This image builds opencv 4.2. How would I be able to upgrade to 4.4?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2). I also use "Qt5GstreamerUi-1.0, Qt5GstreamerUtils-1.0, gstreamer-1.0 and gstreamer1.0-app" packages in the application. What would I need to add to my local.conf in order to get these packages on the IMX8?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 16:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1196598#M166190</guid>
      <dc:creator>rthomas</dc:creator>
      <dc:date>2020-12-09T16:07:59Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCV Packages with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1197438#M166262</link>
      <description>&lt;P&gt;Hello rthomas,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) yes it will work&lt;/P&gt;
&lt;P&gt;2) For example&lt;/P&gt;
&lt;H2&gt;&lt;SPAN class="mw-headline"&gt;Add QtWebKit examples to the build&lt;/SPAN&gt;&lt;/H2&gt;
&lt;P&gt;Add the following line to YOCTO_DIR/BUILD_DIR/conf/local.conf:&lt;/P&gt;
&lt;PRE&gt;IMAGE_INSTALL_append = " qtwebkit-examples-examples"
&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;H2&gt;&lt;SPAN class="mw-headline"&gt;Add QtWebEngine examples to the build&lt;/SPAN&gt;&lt;/H2&gt;
&lt;P&gt;Add the following line to YOCTO_DIR/BUILD_DIR/conf/local.conf:&lt;/P&gt;
&lt;PRE&gt;IMAGE_INSTALL_append = " qtwebengine-examples"
&lt;BR /&gt;Regards
&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 14:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1197438#M166262</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-12-10T14:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCV Packages with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1197521#M166273</link>
      <description>&lt;P&gt;Installing these will give me&amp;nbsp;&lt;SPAN&gt;Qt5GstreamerUi-1.0, Qt5GstreamerUtils-1.0, gstreamer-1.0 and gstreamer1.0-app packages?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 16:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCV-Packages-with-yocto/m-p/1197521#M166273</guid>
      <dc:creator>rthomas</dc:creator>
      <dc:date>2020-12-10T16:39:22Z</dc:date>
    </item>
  </channel>
</rss>