<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to start Watchdog in Kernel Init Process for IMx6ull based Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-start-Watchdog-in-Kernel-Init-Process-for-IMx6ull-based/m-p/1196220#M166179</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using "Freescale i.MX6 series" based custom board where we need hardware-watchdog (which is available in Imx6ULL SoC) to be enabled during kernel initialization process itself rather to wait for an application service triggers and feeds /dev/watchdog device.&lt;/P&gt;&lt;P&gt;This is needed as our custom board sometimes faces random crashes during kernel boot up event which could not be recovered with any reset triggers.&lt;/P&gt;&lt;P&gt;Placing watchdog in early stage of kernel boot-up would recover board from any crash once its timeout seconds elapsed.&lt;/P&gt;&lt;P&gt;Please help us if you know better tricks on kernel panic/oops/hang issue with self recoverable features (soft/hard restart).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nirav&lt;/P&gt;</description>
    <pubDate>Wed, 09 Dec 2020 09:15:35 GMT</pubDate>
    <dc:creator>niravagrawal</dc:creator>
    <dc:date>2020-12-09T09:15:35Z</dc:date>
    <item>
      <title>How to start Watchdog in Kernel Init Process for IMx6ull based Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-start-Watchdog-in-Kernel-Init-Process-for-IMx6ull-based/m-p/1196220#M166179</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using "Freescale i.MX6 series" based custom board where we need hardware-watchdog (which is available in Imx6ULL SoC) to be enabled during kernel initialization process itself rather to wait for an application service triggers and feeds /dev/watchdog device.&lt;/P&gt;&lt;P&gt;This is needed as our custom board sometimes faces random crashes during kernel boot up event which could not be recovered with any reset triggers.&lt;/P&gt;&lt;P&gt;Placing watchdog in early stage of kernel boot-up would recover board from any crash once its timeout seconds elapsed.&lt;/P&gt;&lt;P&gt;Please help us if you know better tricks on kernel panic/oops/hang issue with self recoverable features (soft/hard restart).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nirav&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 09:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-start-Watchdog-in-Kernel-Init-Process-for-IMx6ull-based/m-p/1196220#M166179</guid>
      <dc:creator>niravagrawal</dc:creator>
      <dc:date>2020-12-09T09:15:35Z</dc:date>
    </item>
  </channel>
</rss>