<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8QM boot ROM and image header information</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194235#M166037</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi experts,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am trying to create an eMMC (and/or SPI) flash image that mimics the format expected by the iMX8QM boot ROM. Note, I'm not intending to use u-boot at all. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The boot ROM would then read the information from the header and set up the system as defined in the header. I'd like to have the boot ROM jump to a known address and launch a Cortex-A53 app.bin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this mechanism possible ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can someone please provide some guidance or explain how to go about this ? How would the flash image be created and what would be its layout ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ravi&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 06 Dec 2020 05:39:27 GMT</pubDate>
    <dc:creator>rkohli2000</dc:creator>
    <dc:date>2020-12-06T05:39:27Z</dc:date>
    <item>
      <title>iMX8QM boot ROM and image header information</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194235#M166037</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi experts,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am trying to create an eMMC (and/or SPI) flash image that mimics the format expected by the iMX8QM boot ROM. Note, I'm not intending to use u-boot at all. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The boot ROM would then read the information from the header and set up the system as defined in the header. I'd like to have the boot ROM jump to a known address and launch a Cortex-A53 app.bin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this mechanism possible ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can someone please provide some guidance or explain how to go about this ? How would the flash image be created and what would be its layout ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ravi&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 06 Dec 2020 05:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194235#M166037</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2020-12-06T05:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM boot ROM and image header information</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194239#M166038</link>
      <description>&lt;P&gt;Hi Ravi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can refer to sect."Creating a SCFW only image", "Creating a Cortex-A image only",&lt;/P&gt;
&lt;P&gt;"Creating a Cortex-M4 image only", "Flash image" on below link :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootable-image/ta-p/1101253" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootable-image/ta-p/1101253&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Chapter 5 System Boot&amp;nbsp; &lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 06 Dec 2020 08:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194239#M166038</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-06T08:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM boot ROM and image header information</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194258#M166046</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for the reference. I see the header information and will experiment with the header info fields. Is there risk of bricking my imx8QM MEK ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd like to load an A53 app at a given SPI / eMMC flash address and run it. Something like using uboot's tftpboot &amp;lt;addr&amp;gt; and bootm &amp;lt;addr&amp;gt;. Can uuu help to do this (without a probe) ? Can you explain the user steps ?&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;</description>
      <pubDate>Sun, 06 Dec 2020 17:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194258#M166046</guid>
      <dc:creator>rkohli2000</dc:creator>
      <dc:date>2020-12-06T17:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM boot ROM and image header information</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194286#M166050</link>
      <description>&lt;P&gt;Hi Ravi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there is no risk of bricking imx8QM MEK.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 01:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-boot-ROM-and-image-header-information/m-p/1194286#M166050</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-07T01:05:36Z</dc:date>
    </item>
  </channel>
</rss>