<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKeep boot logo from u-boot during kernel boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-u-boot-during-kernel-boot/m-p/1192402#M165873</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;during u-boot, I initialize the framebuffer of my i.MX6 board and display a logo.&lt;/P&gt;&lt;P&gt;The problem is as soon as kernel starts, screen turns black until framebuffer is initialized.&lt;/P&gt;&lt;P&gt;Is it possible to keep the framebuffer unchanged during kernel boot so I can keep the logo displayed?&lt;/P&gt;&lt;P&gt;Setting the boot logo during kernel boot is not possible because the boot logo needs to be dynamic and not statically compiled into kernel.&lt;/P&gt;</description>
    <pubDate>Wed, 02 Dec 2020 14:30:46 GMT</pubDate>
    <dc:creator>david_schmidt</dc:creator>
    <dc:date>2020-12-02T14:30:46Z</dc:date>
    <item>
      <title>Keep boot logo from u-boot during kernel boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-u-boot-during-kernel-boot/m-p/1192402#M165873</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;during u-boot, I initialize the framebuffer of my i.MX6 board and display a logo.&lt;/P&gt;&lt;P&gt;The problem is as soon as kernel starts, screen turns black until framebuffer is initialized.&lt;/P&gt;&lt;P&gt;Is it possible to keep the framebuffer unchanged during kernel boot so I can keep the logo displayed?&lt;/P&gt;&lt;P&gt;Setting the boot logo during kernel boot is not possible because the boot logo needs to be dynamic and not statically compiled into kernel.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 14:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-u-boot-during-kernel-boot/m-p/1192402#M165873</guid>
      <dc:creator>david_schmidt</dc:creator>
      <dc:date>2020-12-02T14:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Keep boot logo from u-boot during kernel boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-u-boot-during-kernel-boot/m-p/1192713#M165893</link>
      <description>&lt;P&gt;Hi david_schmidt&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try logo patches from&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-uboot-to-kernel-for-NXP/ta-p/1120770" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-uboot-to-kernel-for-NXP/ta-p/1120770&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 00:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-u-boot-during-kernel-boot/m-p/1192713#M165893</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-03T00:26:22Z</dc:date>
    </item>
  </channel>
</rss>