<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUpgrade to Linux kernel 5.9.11 Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Upgrade-to-Linux-kernel-5-9-11-Problem/m-p/1192377#M165869</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;NXP until this moment has the latest release which is 5.4.47.&lt;/P&gt;&lt;P&gt;I'm working on some modules like &lt;STRONG&gt;SN65DSI86&lt;/STRONG&gt; and &lt;STRONG&gt;ov5647&lt;/STRONG&gt; raspberry camera and their drivers are updates in the &lt;STRONG&gt;5.9.10&lt;/STRONG&gt; or &lt;STRONG&gt;5.9.11&lt;/STRONG&gt; Linux kernel.&lt;/P&gt;&lt;P&gt;I looked into &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/&lt;/A&gt; and it seems there is a tag for 5.9.11 &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tag/?h=v5.9.11" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tag/?h=v5.9.11&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I tried to create a recipe similar to the &lt;STRONG&gt;linux-imx_5.4.bb&lt;/STRONG&gt; trying to upgrade to 5.9.11 but it failed fetching.&lt;/P&gt;&lt;P&gt;Can you help me with a recipe to upgrade the kernel?&lt;/P&gt;&lt;P&gt;Thanks, Talel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Dec 2020 13:49:31 GMT</pubDate>
    <dc:creator>talel_hajsalem</dc:creator>
    <dc:date>2020-12-02T13:49:31Z</dc:date>
    <item>
      <title>Upgrade to Linux kernel 5.9.11 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Upgrade-to-Linux-kernel-5-9-11-Problem/m-p/1192377#M165869</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;NXP until this moment has the latest release which is 5.4.47.&lt;/P&gt;&lt;P&gt;I'm working on some modules like &lt;STRONG&gt;SN65DSI86&lt;/STRONG&gt; and &lt;STRONG&gt;ov5647&lt;/STRONG&gt; raspberry camera and their drivers are updates in the &lt;STRONG&gt;5.9.10&lt;/STRONG&gt; or &lt;STRONG&gt;5.9.11&lt;/STRONG&gt; Linux kernel.&lt;/P&gt;&lt;P&gt;I looked into &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/&lt;/A&gt; and it seems there is a tag for 5.9.11 &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tag/?h=v5.9.11" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tag/?h=v5.9.11&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I tried to create a recipe similar to the &lt;STRONG&gt;linux-imx_5.4.bb&lt;/STRONG&gt; trying to upgrade to 5.9.11 but it failed fetching.&lt;/P&gt;&lt;P&gt;Can you help me with a recipe to upgrade the kernel?&lt;/P&gt;&lt;P&gt;Thanks, Talel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Dec 2020 13:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Upgrade-to-Linux-kernel-5-9-11-Problem/m-p/1192377#M165869</guid>
      <dc:creator>talel_hajsalem</dc:creator>
      <dc:date>2020-12-02T13:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrade to Linux kernel 5.9.11 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Upgrade-to-Linux-kernel-5-9-11-Problem/m-p/1193282#M165935</link>
      <description>&lt;P&gt;Hello Talel,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The L5.9.11 still on development and something may not work use the L5.4.47 instead, now if you want to downground to 4.9.11 you will have to downground the kernel as well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 14:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Upgrade-to-Linux-kernel-5-9-11-Problem/m-p/1193282#M165935</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-12-03T14:15:58Z</dc:date>
    </item>
  </channel>
</rss>