<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Is IMX27 HSM (Hardware Secure Module) supported?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191678#M165784</link>
    <description>&lt;P&gt;Hello txh3157,&lt;/P&gt;
&lt;P&gt;The iMX27 does not include the HSM, The HSM is treated as a further core and can be full run controlled. Furthermore, common debugging of the Host/HSM cores and FLASH programming are possible on processor: MPC57xx and MPC56xx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 01 Dec 2020 14:31:09 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-12-01T14:31:09Z</dc:date>
    <item>
      <title>Is IMX27 HSM (Hardware Secure Module) supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191072#M165727</link>
      <description>&lt;P&gt;Does iMX27 include hardware secure module (HSM) for factory to write X.509 cert/key? Is the SCC the right module to look into? If it is, how to enable it from Yocto BSP's setup?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 19:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191072#M165727</guid>
      <dc:creator>txh3157</dc:creator>
      <dc:date>2020-11-30T19:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: Is IMX27 HSM (Hardware Secure Module) supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191678#M165784</link>
      <description>&lt;P&gt;Hello txh3157,&lt;/P&gt;
&lt;P&gt;The iMX27 does not include the HSM, The HSM is treated as a further core and can be full run controlled. Furthermore, common debugging of the Host/HSM cores and FLASH programming are possible on processor: MPC57xx and MPC56xx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 14:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191678#M165784</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-12-01T14:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: Is IMX27 HSM (Hardware Secure Module) supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191765#M165793</link>
      <description>&lt;P&gt;It is not possible for us to change schematic. In the iMX Linux reference doc, does these commands working in iMX27: sm_init_keystore, sm_detect_keystore_units, sm_establish_keystore etc under CAAM module? Can SCC module to be used by application?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 18:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-IMX27-HSM-Hardware-Secure-Module-supported/m-p/1191765#M165793</guid>
      <dc:creator>txh3157</dc:creator>
      <dc:date>2020-12-01T18:11:18Z</dc:date>
    </item>
  </channel>
</rss>