<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux reboot problem watchdog software reset</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-reboot-problem-watchdog-software-reset/m-p/1191557#M165773</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are working on imx6sx custom board running yocto zeus on that. we are facing the reboot freeze issue sometime when we are doing the soft reboot.&lt;/P&gt;&lt;P&gt;Sometimes board reboot but sometimes it stuck once it called the watchdog.&lt;/P&gt;&lt;P&gt;As a fix, just commenting out the following in arch/arm/boot/dts/imx6sx-sdb.dtsi from the linux kernel&lt;/P&gt;&lt;P&gt;&amp;amp;wdog1 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_wdog&amp;gt;;&lt;BR /&gt;// fsl,ext-reset-output;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;It will make only the software reset. So whenever you reboot, you will have only software components restarting.&lt;/P&gt;&lt;P&gt;if that would be ok? For example, is there a strict requirement for Hardware reset, everytime when a user initiates a system restart.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should we have to move with this fix?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nikhil&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 01 Dec 2020 10:48:29 GMT</pubDate>
    <dc:creator>nikhil_sahu2</dc:creator>
    <dc:date>2020-12-01T10:48:29Z</dc:date>
    <item>
      <title>Linux reboot problem watchdog software reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-reboot-problem-watchdog-software-reset/m-p/1191557#M165773</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are working on imx6sx custom board running yocto zeus on that. we are facing the reboot freeze issue sometime when we are doing the soft reboot.&lt;/P&gt;&lt;P&gt;Sometimes board reboot but sometimes it stuck once it called the watchdog.&lt;/P&gt;&lt;P&gt;As a fix, just commenting out the following in arch/arm/boot/dts/imx6sx-sdb.dtsi from the linux kernel&lt;/P&gt;&lt;P&gt;&amp;amp;wdog1 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_wdog&amp;gt;;&lt;BR /&gt;// fsl,ext-reset-output;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;It will make only the software reset. So whenever you reboot, you will have only software components restarting.&lt;/P&gt;&lt;P&gt;if that would be ok? For example, is there a strict requirement for Hardware reset, everytime when a user initiates a system restart.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should we have to move with this fix?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nikhil&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 10:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-reboot-problem-watchdog-software-reset/m-p/1191557#M165773</guid>
      <dc:creator>nikhil_sahu2</dc:creator>
      <dc:date>2020-12-01T10:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: Linux reboot problem watchdog software reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-reboot-problem-watchdog-software-reset/m-p/1194310#M166054</link>
      <description>&lt;P&gt;I think you can comment out the "ext-reset-output" if you don't use the WDOG_B pin.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 02:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-reboot-problem-watchdog-software-reset/m-p/1194310#M166054</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2020-12-07T02:00:01Z</dc:date>
    </item>
  </channel>
</rss>