<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Do you know color corruption issue? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Do-you-know-color-corruption-issue/m-p/228053#M16562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a color corruption issue as attached image.&lt;/P&gt;&lt;P&gt;The bluish-violet part of the image is changed the color from original color.&lt;/P&gt;&lt;P&gt;(Please note that the thoudands of white dot is not issue. These are lots of birds.)&lt;/P&gt;&lt;P&gt;This issue is occurred on MCIMX6Q-SDP and gstreamer in Linux BSP (L3.0.35_4.0.0) when encoding if GOP setting value is large (e.g. gop =15), but it is not occurred unit_test.&lt;/P&gt;&lt;P&gt;Then, we want to know whether same issue was occurred somewhere world wide.&lt;/P&gt;&lt;P&gt;Anyone knows this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jan 2014 09:06:22 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2014-01-10T09:06:22Z</dc:date>
    <item>
      <title>Do you know color corruption issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-you-know-color-corruption-issue/m-p/228053#M16562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a color corruption issue as attached image.&lt;/P&gt;&lt;P&gt;The bluish-violet part of the image is changed the color from original color.&lt;/P&gt;&lt;P&gt;(Please note that the thoudands of white dot is not issue. These are lots of birds.)&lt;/P&gt;&lt;P&gt;This issue is occurred on MCIMX6Q-SDP and gstreamer in Linux BSP (L3.0.35_4.0.0) when encoding if GOP setting value is large (e.g. gop =15), but it is not occurred unit_test.&lt;/P&gt;&lt;P&gt;Then, we want to know whether same issue was occurred somewhere world wide.&lt;/P&gt;&lt;P&gt;Anyone knows this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 09:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-you-know-color-corruption-issue/m-p/228053#M16562</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-01-10T09:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: Do you know color corruption issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-you-know-color-corruption-issue/m-p/228054#M16563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found the root cause of this issue.&lt;/P&gt;&lt;P&gt;It was a height resolution of movie data.&lt;/P&gt;&lt;P&gt;Actually, VPU seems that it does not encode h.264 correctly if height resolution of yuv data is not multiple of 16 when GOP value is large.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, mxc_vpu_test.c in unit_test in L3.0.35_4.1.0 checks the height resolution whether it is multiple of 16 or not.&lt;/P&gt;&lt;P&gt;And if it is not multiple of 16, add some line to the yuv data for changing it to multiple of 16.&lt;/P&gt;&lt;P&gt;On the other hands, gstreamer plug-in (vpuenc.c) for L3.0.35_4.1.0 does not check it, and does not add any line even though it is not multiple of 16.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note this point if you use gstreamer plug-in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jan 2014 01:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-you-know-color-corruption-issue/m-p/228054#M16563</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-01-24T01:16:32Z</dc:date>
    </item>
  </channel>
</rss>