<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6q: PL310 caching issues?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1189679#M165587</link>
    <description>&lt;P&gt;Hi kregl&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;kernel version 3.10.108 is not supported by nxp, but&lt;/P&gt;
&lt;P&gt;some arm errata are fixed by "define CONFIG_ARM_ERRATA" in&lt;/P&gt;
&lt;P&gt;imx_v2014.04 used with linux L3.10.53_1.1.0_ga and one can try them&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6_common.h?h=nxp/imx_v2014.04_3.10.53_1.1.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6_common.h?h=nxp/imx_v2014.04_3.10.53_1.1.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Thu, 26 Nov 2020 11:00:35 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-11-26T11:00:35Z</dc:date>
    <item>
      <title>imx6q: PL310 caching issues?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1189630#M165578</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;We are running an imx6q platform with kernel version 3.10.108.&lt;/P&gt;&lt;P&gt;The error rate increased at the memory stress testing step.&lt;BR /&gt;During this step up to 10 "memtester 35M" processes are spawned and run without core bindings on all 4 cores.&lt;BR /&gt;Attached are multiple memtester log of the same device. All kinds of different subtests of memtester fail from time to time.&lt;/P&gt;&lt;P&gt;Improving memtester to resolve the virtual addresses to physical like so:&lt;BR /&gt;&lt;A href="https://shanetully.com/2014/12/translating-virtual-addresses-to-physcial-addresses-in-user-space/" target="_blank"&gt;https://shanetully.com/2014/12/translating-virtual-addres...&lt;/A&gt;&lt;BR /&gt;showed that the addresses are jumping around, so I think it is no memory problem.&lt;BR /&gt;Binding all processes to a single core or running a single instance with all available memory showed also no problems.&lt;/P&gt;&lt;P&gt;Attached is also the memtester routine for the "Block Sequential" subtest.&lt;BR /&gt;memtester splits the given memory into two buffers and compares them after each memory modification. It looks like the compare steps reads an old value from one buffer.&lt;BR /&gt;Block Sequential : testing 105&lt;BR /&gt;FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d1c.&lt;BR /&gt;The correct value at step 105 is 105 == 0x69 =&amp;gt; 0x69696969&lt;/P&gt;&lt;P&gt;As you can see in the attached failure logs, every failure consists of a contiguous miss match of 8*32bit=32bytes.&lt;BR /&gt;Maybe it has something to do with the PL310 cache, its cacheline consists of 32byte?&lt;BR /&gt;A short test with some newer 4.* kernel did not show this issue. But I have to run it for longer.&lt;BR /&gt;Binding all processes to the same core also solves the issue.&lt;/P&gt;&lt;P&gt;The PL310 driver and the many PL310 ERRATA workarounds were heavily reworked since the 3.10.108 kernel.&lt;BR /&gt;Did anybody suffer from the same issue in the past?&lt;BR /&gt;Can anybody remember which patch fixed the issue and point me in the right direction?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;memtester version 4.3.0 (32-bit)
Copyright (C) 2001-2012 Charles Cazabon.
Licensed under the GNU General Public License version 2 (only).
pagesize is 4096
pagesizemask is 0xfffff000
want 35MB (36700160 bytes)
got 35MB (36700160 bytes), trying mlock ...locked.
Loop 1/1:
Stuck Address : ok
Random Value : ok
Compare XOR : ok
Compare SUB : ok
Compare MUL : ok
Compare DIV : ok
Compare OR : ok
Compare AND : ok
Sequential Increment: ok
Solid Bits : ok
Block Sequential : testing 105
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d1c.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d20.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d24.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d28.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d2c.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d30.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d34.
FAILURE: 0x69696969 != 0x68686868 at offset 0x01045d38.
Checkerboard : ok
Bit Spread : ok
Bit Flip : ok
Walking Ones : ok
Walking Zeroes : ok
8-bit Writes : ok
16-bit Writes : ok
Done.

memtester version 4.3.0 (32-bit)
Copyright (C) 2001-2012 Charles Cazabon.
Licensed under the GNU General Public License version 2 (only).
pagesize is 4096
pagesizemask is 0xfffff000
want 35MB (36700160 bytes)
got 35MB (36700160 bytes), trying mlock ...locked.
Loop 1/1:
Stuck Address : ok
Random Value : ok
Compare XOR : ok
Compare SUB : ok
Compare MUL : ok
Compare DIV : ok
Compare OR : ok
Compare AND : ok
Sequential Increment: ok
Solid Bits : ok
Block Sequential : testing 123
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f00.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f04.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f08.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f0c.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f10.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f14.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f18.
FAILURE: 0x7a7a7a7a != 0x7b7b7b7b at offset 0x00a60f1c.
Checkerboard : ok
Bit Spread : ok
Bit Flip : ok
Walking Ones : ok
Walking Zeroes : ok
8-bit Writes : ok
16-bit Writes : ok
Done.

memtester version 4.3.0 (32-bit)
Copyright (C) 2001-2012 Charles Cazabon.
Licensed under the GNU General Public License version 2 (only).
pagesize is 4096
pagesizemask is 0xfffff000
want 35MB (36700160 bytes)
got 35MB (36700160 bytes), trying mlock ...locked.
Loop 1/1:
Stuck Address : ok
Random Value : ok
Compare XOR : ok
Compare SUB : ok
Compare MUL : ok
Compare DIV : ok
Compare OR : ok
Compare AND : ok
Sequential Increment: ok
Solid Bits : ok
Block Sequential : testing 247
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb1c.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb20.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb24.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb28.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb2c.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb30.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb34.
FAILURE: 0xf7f7f7f7 != 0xf6f6f6f6 at offset 0x0079bb38.
Checkerboard : ok
Bit Spread : ok
Bit Flip : ok
Walking Ones : ok
Walking Zeroes : ok
8-bit Writes : ok
16-bit Writes : ok
Done.

memtester version 4.3.0 (32-bit)
Copyright (C) 2001-2012 Charles Cazabon.
Licensed under the GNU General Public License version 2 (only).
pagesize is 4096
pagesizemask is 0xfffff000
want 35MB (36700160 bytes)
got 35MB (36700160 bytes), trying mlock ...locked.
Loop 1/1:
Stuck Address : ok
Random Value : ok
Compare XOR : ok
Compare SUB : ok
Compare MUL : ok
Compare DIV : ok
Compare OR : ok
Compare AND : ok
Sequential Increment: ok
Solid Bits : testing 37
FAILURE: 0xffffffff != 0x00000000 at offset 0x0097c27c.
FAILURE: 0x00000000 != 0xffffffff at offset 0x0097c280.
FAILURE: 0xffffffff != 0x00000000 at offset 0x0097c284.
FAILURE: 0x00000000 != 0xffffffff at offset 0x0097c288.
FAILURE: 0xffffffff != 0x00000000 at offset 0x0097c28c.
FAILURE: 0x00000000 != 0xffffffff at offset 0x0097c290.
FAILURE: 0xffffffff != 0x00000000 at offset 0x0097c294.
FAILURE: 0x00000000 != 0xffffffff at offset 0x0097c298.
Block Sequential : ok
Checkerboard : ok
Bit Spread : ok
Bit Flip : ok
Walking Ones : ok
Walking Zeroes : ok
8-bit Writes : ok
16-bit Writes : ok
Done.&lt;/LI-CODE&gt;&lt;LI-CODE lang="c"&gt;int compare_regions(ulv *bufa, ulv *bufb, size_t count) {
int r = 0;
size_t i;
ulv *p1 = bufa;
ulv *p2 = bufb;
off_t physaddr;

for (i = 0; i &amp;lt; count; i++, p1++, p2++) {
if (*p1 != *p2) {
if (use_phys) {
physaddr = physaddrbase + (i * sizeof(ul));
fprintf(stderr,
"FAILURE: 0x%08lx != 0x%08lx at physical address "
"0x%08lx.\n",
(ul) *p1, (ul) *p2, physaddr);
} else {
fprintf(stderr,
"FAILURE: 0x%08lx != 0x%08lx at offset 0x%08lx.\n",
(ul) *p1, (ul) *p2, (ul) (i * sizeof(ul)));
}
/* printf("Skipping to next test..."); */
r = -1;
}
}
return r;
}

int test_blockseq_comparison(ulv *bufa, ulv *bufb, size_t count) {
ulv *p1 = bufa;
ulv *p2 = bufb;
unsigned int j;
size_t i;

printf(" ");
fflush(stdout);
for (j = 0; j &amp;lt; 256; j++) {
printf("\b\b\b\b\b\b\b\b\b\b\b");
p1 = (ulv *) bufa;
p2 = (ulv *) bufb;
printf("setting %3u", j);
fflush(stdout);
for (i = 0; i &amp;lt; count; i++) {
*p1++ = *p2++ = (ul) UL_BYTE(j);
}
printf("\b\b\b\b\b\b\b\b\b\b\b");
printf("testing %3u", j);
fflush(stdout);
if (compare_regions(bufa, bufb, count)) {
return -1;
}
}
printf("\b\b\b\b\b\b\b\b\b\b\b \b\b\b\b\b\b\b\b\b\b\b");
fflush(stdout);
return 0;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 09:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1189630#M165578</guid>
      <dc:creator>kregl</dc:creator>
      <dc:date>2020-11-26T09:57:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q: PL310 caching issues?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1189679#M165587</link>
      <description>&lt;P&gt;Hi kregl&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;kernel version 3.10.108 is not supported by nxp, but&lt;/P&gt;
&lt;P&gt;some arm errata are fixed by "define CONFIG_ARM_ERRATA" in&lt;/P&gt;
&lt;P&gt;imx_v2014.04 used with linux L3.10.53_1.1.0_ga and one can try them&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6_common.h?h=nxp/imx_v2014.04_3.10.53_1.1.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6_common.h?h=nxp/imx_v2014.04_3.10.53_1.1.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 11:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1189679#M165587</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-26T11:00:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q: PL310 caching issues?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1190111#M165629</link>
      <description>&lt;P&gt;The supplied uboot version from the board vendor is 2015.07.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;CONFIG_ARM_ERRATA_845369 is missing in mainline uboot up to some 2017 version.&lt;BR /&gt;But the boardvendor has included this fix in the 2015.07 uboot. All other erratas in your link are also active.&lt;/P&gt;&lt;P&gt;So maybe it hat something to do with a combination uboot+kernel?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Nov 2020 06:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-PL310-caching-issues/m-p/1190111#M165629</guid>
      <dc:creator>kregl</dc:creator>
      <dc:date>2020-11-27T06:59:40Z</dc:date>
    </item>
  </channel>
</rss>