<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where can I find GPU SDK for i.MX8QM? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1189247#M165512</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;First, thanks for helping me.&lt;BR /&gt;Ok, I have download L4.14.98_2.0.0_ga_images_MX8QMMEK.zip and unzip it on an NFS directory. I have unzipped fsl-image-validation-imx-imx8qmmek.tar.bz2 on an NFS folder. I booted the kernel 4.14.170 via TFTP and pointed NFS folder with the fs-image-...l RootFS. Then, I could run all examples on the /opt/imx-gpu-sdk/OpenCL/ folder without any problem.&lt;BR /&gt;I have downloaded the L4.14.98_2.0.0_ga_images_MX8QMMEK.zip from:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So, I can use OpenCL with kernel 4.14.170, and NXP RootFS without any problem.&lt;BR /&gt;I did the same test using a RootFS system from Variscite, that is Debian 10, and the OpenCL is working too.&lt;BR /&gt;&lt;BR /&gt;Now, I have copied the /opt/imx-gpu-sdk and all libraries dependencies to execute the OpenCL/Info example of the NXP on the Debian10, and I getting the following error:&lt;BR /&gt;root@apalis-iMX8:/opt/imx-gpu-sdk/OpenCL/Info# ./Info&lt;BR /&gt;ERROR: clGetPlatformIDs(0, nullptr, &amp;amp;count) failed with error code Unknown (-1001) at source/FslUtil/OpenCL1_1/OpenCLHelper.cpp(121)&lt;/P&gt;&lt;P&gt;and the result to check the Info library dependency is:&lt;BR /&gt;root@apalis-iMX8:/opt/imx-gpu-sdk/OpenCL/Info# ldd Info&lt;BR /&gt;linux-vdso.so.1 (0x0000ffffb051b000)&lt;BR /&gt;libIL.so =&amp;gt; /usr/lib/libIL.so (0x0000ffffb03b7000)&lt;BR /&gt;libOpenCL.so =&amp;gt; /usr/lib/libOpenCL.so (0x0000ffffb03a1000)&lt;BR /&gt;libstdc++.so.6 =&amp;gt; /usr/lib/aarch64-linux-gnu/libstdc++.so.6 (0x0000ffffb0216000)&lt;BR /&gt;libm.so.6 =&amp;gt; /lib/aarch64-linux-gnu/libm.so.6 (0x0000ffffb0159000)&lt;BR /&gt;libgcc_s.so.1 =&amp;gt; /lib/aarch64-linux-gnu/libgcc_s.so.1 (0x0000ffffb0135000)&lt;BR /&gt;libpthread.so.0 =&amp;gt; /lib/aarch64-linux-gnu/libpthread.so.0 (0x0000ffffb0106000)&lt;BR /&gt;libc.so.6 =&amp;gt; /lib/aarch64-linux-gnu/libc.so.6 (0x0000ffffaff94000)&lt;BR /&gt;libpng16.so.16 =&amp;gt; /usr/lib/libpng16.so.16 (0x0000ffffaff59000)&lt;BR /&gt;libjpeg.so.62 =&amp;gt; /usr/lib/libjpeg.so.62 (0x0000ffffaff0f000)&lt;BR /&gt;libtiff.so.5 =&amp;gt; /usr/lib/libtiff.so.5 (0x0000ffffafe93000)&lt;BR /&gt;libdl.so.2 =&amp;gt; /lib/aarch64-linux-gnu/libdl.so.2 (0x0000ffffafe7f000)&lt;BR /&gt;librt.so.1 =&amp;gt; /lib/aarch64-linux-gnu/librt.so.1 (0x0000ffffafe67000)&lt;BR /&gt;/lib/ld-linux-aarch64.so.1 (0x0000ffffb04ed000)&lt;BR /&gt;libz.so.1 =&amp;gt; /lib/aarch64-linux-gnu/libz.so.1 (0x0000ffffafe3a000)&lt;BR /&gt;liblzma.so.5 =&amp;gt; /lib/aarch64-linux-gnu/liblzma.so.5 (0x0000ffffafe05000)&lt;/P&gt;&lt;P&gt;Probably, I am missing some configuration.&lt;BR /&gt;Now, I am reading the i.MX Linux Reference Manual.pdf to try to find something to fix this issue.&lt;BR /&gt;&lt;BR /&gt;Is the Vivante package for i.MX8QM created by Yocto?&lt;BR /&gt;Maybe, I can take a look on the recipes or repository to see what I am missing!&lt;BR /&gt;Do you know what is the repository for the Vivante packages for i.MX8QM?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 25 Nov 2020 19:09:16 GMT</pubDate>
    <dc:creator>gabrielaugustoc</dc:creator>
    <dc:date>2020-11-25T19:09:16Z</dc:date>
    <item>
      <title>Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1186830#M165309</link>
      <description>&lt;P&gt;Hi, I would like to use OpenCL with i.MX8QM and I could not find the libraries and compiler for Vivante GC7000/XSVX GPGPU.&lt;BR /&gt;I have found on the i.MX Linux Reference Manual, page 166, the list of libraries for the GPU, but I did not find which libraries are for the i.MX8QM, how to get and install them.&lt;BR /&gt;My kernel version is 4.14.170 and I am using Debian 9 for Arm64.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Nov 2020 17:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1186830#M165309</guid>
      <dc:creator>gabrielaugustoc</dc:creator>
      <dc:date>2020-11-20T17:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1187555#M165374</link>
      <description>&lt;P&gt;Hello gabriel,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The reason is because you are no using an nxp correct kernel version you must use 4.9.88 or 5.4.24BSP to have all the GPU libraries on it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 15:00:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1187555#M165374</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-11-23T15:00:42Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1187672#M165384</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;BR /&gt;But, this will be a problem for me because I have added some image sensors drivers in the 4.14.170 Kernel. This is a branch from Toradex.&lt;BR /&gt;Is there another way to get the source code for these libraries and compile it for my Kernel?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Gabriel&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 18:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1187672#M165384</guid>
      <dc:creator>gabrielaugustoc</dc:creator>
      <dc:date>2020-11-23T18:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1188324#M165441</link>
      <description>&lt;P&gt;Hello Gabriel,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately no from NXP, but you can consult with Toradex if they have it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 16:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1188324#M165441</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-11-24T16:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1189247#M165512</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;First, thanks for helping me.&lt;BR /&gt;Ok, I have download L4.14.98_2.0.0_ga_images_MX8QMMEK.zip and unzip it on an NFS directory. I have unzipped fsl-image-validation-imx-imx8qmmek.tar.bz2 on an NFS folder. I booted the kernel 4.14.170 via TFTP and pointed NFS folder with the fs-image-...l RootFS. Then, I could run all examples on the /opt/imx-gpu-sdk/OpenCL/ folder without any problem.&lt;BR /&gt;I have downloaded the L4.14.98_2.0.0_ga_images_MX8QMMEK.zip from:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So, I can use OpenCL with kernel 4.14.170, and NXP RootFS without any problem.&lt;BR /&gt;I did the same test using a RootFS system from Variscite, that is Debian 10, and the OpenCL is working too.&lt;BR /&gt;&lt;BR /&gt;Now, I have copied the /opt/imx-gpu-sdk and all libraries dependencies to execute the OpenCL/Info example of the NXP on the Debian10, and I getting the following error:&lt;BR /&gt;root@apalis-iMX8:/opt/imx-gpu-sdk/OpenCL/Info# ./Info&lt;BR /&gt;ERROR: clGetPlatformIDs(0, nullptr, &amp;amp;count) failed with error code Unknown (-1001) at source/FslUtil/OpenCL1_1/OpenCLHelper.cpp(121)&lt;/P&gt;&lt;P&gt;and the result to check the Info library dependency is:&lt;BR /&gt;root@apalis-iMX8:/opt/imx-gpu-sdk/OpenCL/Info# ldd Info&lt;BR /&gt;linux-vdso.so.1 (0x0000ffffb051b000)&lt;BR /&gt;libIL.so =&amp;gt; /usr/lib/libIL.so (0x0000ffffb03b7000)&lt;BR /&gt;libOpenCL.so =&amp;gt; /usr/lib/libOpenCL.so (0x0000ffffb03a1000)&lt;BR /&gt;libstdc++.so.6 =&amp;gt; /usr/lib/aarch64-linux-gnu/libstdc++.so.6 (0x0000ffffb0216000)&lt;BR /&gt;libm.so.6 =&amp;gt; /lib/aarch64-linux-gnu/libm.so.6 (0x0000ffffb0159000)&lt;BR /&gt;libgcc_s.so.1 =&amp;gt; /lib/aarch64-linux-gnu/libgcc_s.so.1 (0x0000ffffb0135000)&lt;BR /&gt;libpthread.so.0 =&amp;gt; /lib/aarch64-linux-gnu/libpthread.so.0 (0x0000ffffb0106000)&lt;BR /&gt;libc.so.6 =&amp;gt; /lib/aarch64-linux-gnu/libc.so.6 (0x0000ffffaff94000)&lt;BR /&gt;libpng16.so.16 =&amp;gt; /usr/lib/libpng16.so.16 (0x0000ffffaff59000)&lt;BR /&gt;libjpeg.so.62 =&amp;gt; /usr/lib/libjpeg.so.62 (0x0000ffffaff0f000)&lt;BR /&gt;libtiff.so.5 =&amp;gt; /usr/lib/libtiff.so.5 (0x0000ffffafe93000)&lt;BR /&gt;libdl.so.2 =&amp;gt; /lib/aarch64-linux-gnu/libdl.so.2 (0x0000ffffafe7f000)&lt;BR /&gt;librt.so.1 =&amp;gt; /lib/aarch64-linux-gnu/librt.so.1 (0x0000ffffafe67000)&lt;BR /&gt;/lib/ld-linux-aarch64.so.1 (0x0000ffffb04ed000)&lt;BR /&gt;libz.so.1 =&amp;gt; /lib/aarch64-linux-gnu/libz.so.1 (0x0000ffffafe3a000)&lt;BR /&gt;liblzma.so.5 =&amp;gt; /lib/aarch64-linux-gnu/liblzma.so.5 (0x0000ffffafe05000)&lt;/P&gt;&lt;P&gt;Probably, I am missing some configuration.&lt;BR /&gt;Now, I am reading the i.MX Linux Reference Manual.pdf to try to find something to fix this issue.&lt;BR /&gt;&lt;BR /&gt;Is the Vivante package for i.MX8QM created by Yocto?&lt;BR /&gt;Maybe, I can take a look on the recipes or repository to see what I am missing!&lt;BR /&gt;Do you know what is the repository for the Vivante packages for i.MX8QM?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 19:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1189247#M165512</guid>
      <dc:creator>gabrielaugustoc</dc:creator>
      <dc:date>2020-11-25T19:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1189778#M165593</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You must configure your kernel and pass as module the GPU.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 14:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1189778#M165593</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-11-26T14:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: Where can I find GPU SDK for i.MX8QM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1190407#M165655</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;So, the simplest solution to use OpenCL on Debian for i.MX8QM, take the blue pill, and use the Debian10 RootFS from Variscite:&lt;BR /&gt;&lt;A href="ftp://ftp.variscite.com/VAR-SOM-MX8/Software/debian/" target="_blank"&gt;ftp://ftp.variscite.com/VAR-SOM-MX8/Software/debian/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Mount this image as a loop in the memory system, then compress with tar, and install where you want.&lt;BR /&gt;Thank Variscite for the amazing job.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Gabriel&lt;/P&gt;</description>
      <pubDate>Fri, 27 Nov 2020 19:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-can-I-find-GPU-SDK-for-i-MX8QM/m-p/1190407#M165655</guid>
      <dc:creator>gabrielaugustoc</dc:creator>
      <dc:date>2020-11-27T19:24:51Z</dc:date>
    </item>
  </channel>
</rss>