<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8M LPDDR4 RPA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-LPDDR4-RPA/m-p/1185046#M165089</link>
    <description>&lt;P&gt;I have two questions about the&amp;nbsp;iMX8M RPA&amp;nbsp; LPDDR4 calculation sheet.&lt;/P&gt;&lt;P&gt;1) In the&amp;nbsp;DDRC_INIT7 register the&amp;nbsp;LPDDR4 MR22: ODTE-CS field is set to '1'. If I'm correct than this means that the ODT is disabled for the CS signal in the LPDDR4 device.&lt;/P&gt;&lt;P&gt;What is the reason to only disable the ODT for the CS signals?&lt;/P&gt;&lt;P&gt;2) I discovered that the maximum row address setting for the iMX8M is 16. this means that a single rank memory configuration is limited to 8Gbit per channel. This limitation is not described in the documentation and in the RPA calculation sheet. can this be added?&lt;/P&gt;</description>
    <pubDate>Wed, 18 Nov 2020 08:25:01 GMT</pubDate>
    <dc:creator>jeroenvanandel</dc:creator>
    <dc:date>2020-11-18T08:25:01Z</dc:date>
    <item>
      <title>iMX8M LPDDR4 RPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-LPDDR4-RPA/m-p/1185046#M165089</link>
      <description>&lt;P&gt;I have two questions about the&amp;nbsp;iMX8M RPA&amp;nbsp; LPDDR4 calculation sheet.&lt;/P&gt;&lt;P&gt;1) In the&amp;nbsp;DDRC_INIT7 register the&amp;nbsp;LPDDR4 MR22: ODTE-CS field is set to '1'. If I'm correct than this means that the ODT is disabled for the CS signal in the LPDDR4 device.&lt;/P&gt;&lt;P&gt;What is the reason to only disable the ODT for the CS signals?&lt;/P&gt;&lt;P&gt;2) I discovered that the maximum row address setting for the iMX8M is 16. this means that a single rank memory configuration is limited to 8Gbit per channel. This limitation is not described in the documentation and in the RPA calculation sheet. can this be added?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 08:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-LPDDR4-RPA/m-p/1185046#M165089</guid>
      <dc:creator>jeroenvanandel</dc:creator>
      <dc:date>2020-11-18T08:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M LPDDR4 RPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-LPDDR4-RPA/m-p/1227874#M169128</link>
      <description>&lt;P&gt;Recommend you to use the support value in the script.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 10:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-LPDDR4-RPA/m-p/1227874#M169128</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-02-08T10:15:05Z</dc:date>
    </item>
  </channel>
</rss>