<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 RGMII voltage tolerance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-RGMII-voltage-tolerance/m-p/1184916#M165064</link>
    <description>&lt;P&gt;Hi, Experts&lt;/P&gt;&lt;P&gt;We have a AR8031(PHY) which RGMII IO voltage(VDDIO_REG) is 1.8V, and the IMX6 use the 1.5V for the NVCC_RGMII.&lt;/P&gt;&lt;P&gt;AR8031 RGMII IO voltage seems could not be set to 1.5V.&lt;/P&gt;&lt;P&gt;My question is, could the IMX6 1.5v RGMII interface compatible with the PHY's 1.8V ?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 18 Nov 2020 05:18:36 GMT</pubDate>
    <dc:creator>mcggoal</dc:creator>
    <dc:date>2020-11-18T05:18:36Z</dc:date>
    <item>
      <title>IMX6 RGMII voltage tolerance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-RGMII-voltage-tolerance/m-p/1184916#M165064</link>
      <description>&lt;P&gt;Hi, Experts&lt;/P&gt;&lt;P&gt;We have a AR8031(PHY) which RGMII IO voltage(VDDIO_REG) is 1.8V, and the IMX6 use the 1.5V for the NVCC_RGMII.&lt;/P&gt;&lt;P&gt;AR8031 RGMII IO voltage seems could not be set to 1.5V.&lt;/P&gt;&lt;P&gt;My question is, could the IMX6 1.5v RGMII interface compatible with the PHY's 1.8V ?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 05:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-RGMII-voltage-tolerance/m-p/1184916#M165064</guid>
      <dc:creator>mcggoal</dc:creator>
      <dc:date>2020-11-18T05:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 RGMII voltage tolerance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-RGMII-voltage-tolerance/m-p/1184998#M165079</link>
      <description>&lt;P&gt;Hi mcggoal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at datasheet of used device, for example for i.MX6Q&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/130364i8932CD2A7290E0D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;so for PHY's 1.8V&amp;nbsp; it is necessary to use NVCC_RGMII 1.70V-1.90V&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 07:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-RGMII-voltage-tolerance/m-p/1184998#M165079</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-18T07:00:56Z</dc:date>
    </item>
  </channel>
</rss>