<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8M Mini: SPI-bus native CS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1184394#M165006</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to ask NXP experts about SPI (ECSPI). My company is switching to iMX8 and in order to desighn the HW we need to know these details.&lt;/P&gt;&lt;P&gt;I've been studying&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;IMX8MMRM.pdf&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;8.1&amp;nbsp;External Signals and Pin Multiplexing&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 10.1&amp;nbsp;Enhanced Configurable SPI (ECSPI)&amp;nbsp;&lt;/P&gt;&lt;P&gt;And asked my EVA- manufacturer but have not got an answer:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; How are SPI chip selects SS1, SS2 and SS3 muxed to hardware pins, (or balls or pads - which way ever one calls them) ??&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I heard that NXP is recommending to use gpio for chip selects (in Linux??) - is that true and if is, why?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Risto H.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Nov 2020 09:17:50 GMT</pubDate>
    <dc:creator>ristohedman</dc:creator>
    <dc:date>2020-11-17T09:17:50Z</dc:date>
    <item>
      <title>i.MX 8M Mini: SPI-bus native CS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1184394#M165006</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to ask NXP experts about SPI (ECSPI). My company is switching to iMX8 and in order to desighn the HW we need to know these details.&lt;/P&gt;&lt;P&gt;I've been studying&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;IMX8MMRM.pdf&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;8.1&amp;nbsp;External Signals and Pin Multiplexing&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 10.1&amp;nbsp;Enhanced Configurable SPI (ECSPI)&amp;nbsp;&lt;/P&gt;&lt;P&gt;And asked my EVA- manufacturer but have not got an answer:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; How are SPI chip selects SS1, SS2 and SS3 muxed to hardware pins, (or balls or pads - which way ever one calls them) ??&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I heard that NXP is recommending to use gpio for chip selects (in Linux??) - is that true and if is, why?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Risto H.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Nov 2020 09:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1184394#M165006</guid>
      <dc:creator>ristohedman</dc:creator>
      <dc:date>2020-11-17T09:17:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini: SPI-bus native CS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1184966#M165076</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/136895"&gt;@ristohedman&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; Customers can use Table 8-1 (Muxing Options) of the i.MX8Mm RM.&lt;BR /&gt;As for pin assignments - use section 5 (Package information and contact assignments)&lt;BR /&gt;of i.MX8Mm Datasheet.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf &lt;/A&gt;&lt;/P&gt;
&lt;P&gt;GPIO instead of "native" SS may be used for non supported modes, say for "long"&lt;BR /&gt;messages.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 06:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1184966#M165076</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-11-18T06:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini: SPI-bus native CS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185231#M165117</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Hmmm, now I must have a great misunderstanding, if I try to search e.g. ECSPI1_SS1 in any 'mini'- related document, I can not find ??!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;br, ristoH&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 13:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185231#M165117</guid>
      <dc:creator>ristohedman</dc:creator>
      <dc:date>2020-11-18T13:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini: SPI-bus native CS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185723#M165172</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/136895"&gt;@ristohedman&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;i.MX8Mm supports single eCSPI SS: ECSPI1_SS0 - there are no more (ECSPI1_SS1 ...).&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-can-I-use-ECSPI-SS1-2/m-p/848467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-can-I-use-ECSPI-SS1-2/m-p/848467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 04:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185723#M165172</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-11-19T04:15:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini: SPI-bus native CS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185787#M165178</link>
      <description>&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;Finally an answer - not a good one for me but answer anyway.&lt;/P&gt;&lt;P&gt;BR, ristoH&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 07:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-SPI-bus-native-CS/m-p/1185787#M165178</guid>
      <dc:creator>ristohedman</dc:creator>
      <dc:date>2020-11-19T07:17:44Z</dc:date>
    </item>
  </channel>
</rss>