<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックImx8 Demo Capacitor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1181370#M164776</link>
    <description>&lt;P&gt;Hi at all,&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;in the demo board and exacly IMX8QM POWER sheet, are reported some pair of capacitor in parallel connection with same value but different work voltage; i saw also the impedance comparison function of frequency but are the same, for example C372 2.2uF 10V and C378 2.2uF 6.3V why this selection? instead to use 2 capacitor of same work voltage?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;</description>
    <pubDate>Wed, 11 Nov 2020 09:01:33 GMT</pubDate>
    <dc:creator>FilippoDeveloper</dc:creator>
    <dc:date>2020-11-11T09:01:33Z</dc:date>
    <item>
      <title>Imx8 Demo Capacitor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1181370#M164776</link>
      <description>&lt;P&gt;Hi at all,&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;in the demo board and exacly IMX8QM POWER sheet, are reported some pair of capacitor in parallel connection with same value but different work voltage; i saw also the impedance comparison function of frequency but are the same, for example C372 2.2uF 10V and C378 2.2uF 6.3V why this selection? instead to use 2 capacitor of same work voltage?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 09:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1181370#M164776</guid>
      <dc:creator>FilippoDeveloper</dc:creator>
      <dc:date>2020-11-11T09:01:33Z</dc:date>
    </item>
    <item>
      <title>Re: Imx8 Demo Capacitor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1181917#M164804</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I discussed your question with i.MX Expert. Here are some explanations and suggestions for you:&lt;BR /&gt;1. For these capacitors, in your own design, you can choose either 10V or 6.3V according to the output voltage.&lt;BR /&gt;2. On the board, for the 3.3V IO power supply, we recommend using a 10V capacitor.&lt;/P&gt;
&lt;P&gt;In order to unify the components on the board, we recommend that you use 10V capacitors.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;[comment]&lt;/STRONG&gt;&lt;BR /&gt;For other power supply circuits, all capacitors can be selected according to the power supply output voltage.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this information is helpful to you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;Weidong&lt;/P&gt;</description>
      <pubDate>Thu, 12 Nov 2020 02:50:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1181917#M164804</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-11-12T02:50:17Z</dc:date>
    </item>
    <item>
      <title>Re: Imx8 Demo Capacitor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1182197#M164827</link>
      <description>&lt;P&gt;Ok, thanks for your reply. I think that double choose possibility was for a new engineering project...perhaps..&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Nov 2020 09:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx8-Demo-Capacitor/m-p/1182197#M164827</guid>
      <dc:creator>FilippoDeveloper</dc:creator>
      <dc:date>2020-11-12T09:32:47Z</dc:date>
    </item>
  </channel>
</rss>