<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8MM. CCM OUTPUT</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-CCM-OUTPUT/m-p/1179744#M164628</link>
    <description>&lt;P&gt;Hello, I am designing a custom board using i.MX8MM.&lt;/P&gt;&lt;P&gt;There are four different ICs that need External Xtal for proper operations.&lt;/P&gt;&lt;P&gt;KSZ9131RNXC Ethernet PHY needs 25 MHz Clock Input.&lt;/P&gt;&lt;P&gt;DSI to HDMI converter needs 25MHz clock Input.&lt;/P&gt;&lt;P&gt;USB HUB needs 12 MHz clock input.&lt;/P&gt;&lt;P&gt;Do I have to use external XTAL for all ICs or can I provide the necessary clock input from&amp;nbsp;i.MX8MM CCM outputs.&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;From the application note what I understood The SoC can provide external clock output using&amp;nbsp;&lt;/P&gt;&lt;P&gt;CCM pins. Is that possible to provide all these clock inputs from these pins and how can I set them&lt;/P&gt;&lt;P&gt;And Do you have any idea about clock integrity as a PPM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ccm.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/129377i97E02DDED208205B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ccm.PNG" alt="ccm.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 08 Nov 2020 11:49:59 GMT</pubDate>
    <dc:creator>EErdem</dc:creator>
    <dc:date>2020-11-08T11:49:59Z</dc:date>
    <item>
      <title>i.MX8MM. CCM OUTPUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-CCM-OUTPUT/m-p/1179744#M164628</link>
      <description>&lt;P&gt;Hello, I am designing a custom board using i.MX8MM.&lt;/P&gt;&lt;P&gt;There are four different ICs that need External Xtal for proper operations.&lt;/P&gt;&lt;P&gt;KSZ9131RNXC Ethernet PHY needs 25 MHz Clock Input.&lt;/P&gt;&lt;P&gt;DSI to HDMI converter needs 25MHz clock Input.&lt;/P&gt;&lt;P&gt;USB HUB needs 12 MHz clock input.&lt;/P&gt;&lt;P&gt;Do I have to use external XTAL for all ICs or can I provide the necessary clock input from&amp;nbsp;i.MX8MM CCM outputs.&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;From the application note what I understood The SoC can provide external clock output using&amp;nbsp;&lt;/P&gt;&lt;P&gt;CCM pins. Is that possible to provide all these clock inputs from these pins and how can I set them&lt;/P&gt;&lt;P&gt;And Do you have any idea about clock integrity as a PPM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ccm.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/129377i97E02DDED208205B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ccm.PNG" alt="ccm.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 08 Nov 2020 11:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-CCM-OUTPUT/m-p/1179744#M164628</guid>
      <dc:creator>EErdem</dc:creator>
      <dc:date>2020-11-08T11:49:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MM. CCM OUTPUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-CCM-OUTPUT/m-p/1179767#M164634</link>
      <description>&lt;P&gt;Hi EErdem&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for external clock output using CCM one can look at imx8mm-evk.dts :&lt;/P&gt;
&lt;P&gt;pinctrl_csi_rst: csi_rst_grp {&lt;BR /&gt;&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_GPIO1_IO14_CCMSRCGPCMIX_CLKO1 0x59&lt;BR /&gt;ov5640_mipi: ov5640_mipi@3c {&lt;BR /&gt;..&amp;lt;&amp;amp;pinctrl_csi_rst&amp;gt;;&lt;BR /&gt;&lt;BR /&gt;clocks = &amp;lt;&amp;amp;clk IMX8MM_CLK_CLKO1&amp;gt;;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm-evk.dts?h=imx_5.4.47_2.2.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm-evk.dts?h=imx_5.4.47_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Output clock stability (ppm) is defined by used crystal.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 09 Nov 2020 01:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-CCM-OUTPUT/m-p/1179767#M164634</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-09T01:11:47Z</dc:date>
    </item>
  </channel>
</rss>