<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Getting HABv4 spl offset from boot image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Getting-HABv4-spl-offset-from-boot-image/m-p/1178698#M164556</link>
    <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;I'm enabling HABv4 secure-boot on imx8mm. As usual, need an SPL hab block to create the CSF descriptor file e.g&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Blocks = 0x7e0fd0 0x1a000 0x2e600 "flash.bin"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works totally fine when we do all the signing steps manually. But to automate the signing process with Yocto there is an issue. It is possible that the build gets complete from caches, without generating build logs.&lt;/P&gt;&lt;P&gt;So, is there any way to get this spl hab block offset value directly from the boot image? or similar, like we can print fit block values?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ make SOC=&amp;lt;SoC Name&amp;gt; print_fit_hab&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 05 Nov 2020 10:27:02 GMT</pubDate>
    <dc:creator>sajjadahmed</dc:creator>
    <dc:date>2020-11-05T10:27:02Z</dc:date>
    <item>
      <title>Getting HABv4 spl offset from boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-HABv4-spl-offset-from-boot-image/m-p/1178698#M164556</link>
      <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;I'm enabling HABv4 secure-boot on imx8mm. As usual, need an SPL hab block to create the CSF descriptor file e.g&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Blocks = 0x7e0fd0 0x1a000 0x2e600 "flash.bin"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works totally fine when we do all the signing steps manually. But to automate the signing process with Yocto there is an issue. It is possible that the build gets complete from caches, without generating build logs.&lt;/P&gt;&lt;P&gt;So, is there any way to get this spl hab block offset value directly from the boot image? or similar, like we can print fit block values?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ make SOC=&amp;lt;SoC Name&amp;gt; print_fit_hab&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 10:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-HABv4-spl-offset-from-boot-image/m-p/1178698#M164556</guid>
      <dc:creator>sajjadahmed</dc:creator>
      <dc:date>2020-11-05T10:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: Getting HABv4 spl offset from boot image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-HABv4-spl-offset-from-boot-image/m-p/1181266#M164765</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/117848"&gt;@sajjadahmed&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;The following document provides i.MX8M, i.MX8MM Secure Boot guide.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_mx8mm_secure_boot.txt?h=imx_v2018.03_4.14.98_2.1.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_mx8mm_secure_boot.txt?h=imx_v2018.03_4.14.98_2.1.0 &lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We do not have automation tools for secure boot images creation.&lt;BR /&gt;Customers can design own scripts to analyze the build logs in order&lt;BR /&gt;to generate signed boot images.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 06:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-HABv4-spl-offset-from-boot-image/m-p/1181266#M164765</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-11-11T06:59:02Z</dc:date>
    </item>
  </channel>
</rss>