<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6ULL Booting error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-Booting-error/m-p/1177722#M164497</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have designed an board with iMX6ULL. The board is powered ON successfully and while booting, the below pint is displayed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-nxp/imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Nov 02 2020 - 12:48:26 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.1 69 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 55C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: i.MX6ULL iW-RAINBOW-G18M-SM&lt;BR /&gt;Boot Device: NAND&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=0&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=1&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=2&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x21a0000&lt;BR /&gt;Can't find PMIC:PFUZE3000&lt;BR /&gt;initcall sequence 8ff91a8c failed at call 87804914 (err=-1)&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried resetting the board multiple times and observed same print.&lt;/P&gt;&lt;P&gt;One of the GPIO (E5 pin of CPU - CSI_PIXCLK) we are using for enabling peripheral power control for the switch. By default the GPIO is externally pulled down.&lt;/P&gt;&lt;P&gt;When the external pulldown is removed for the same GPIO, the board is successfully booting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly let me know what is the reason for such error when the pin is pulled down.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Nibin&lt;/P&gt;</description>
    <pubDate>Wed, 04 Nov 2020 06:59:10 GMT</pubDate>
    <dc:creator>NibinDasS</dc:creator>
    <dc:date>2020-11-04T06:59:10Z</dc:date>
    <item>
      <title>iMX6ULL Booting error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-Booting-error/m-p/1177722#M164497</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have designed an board with iMX6ULL. The board is powered ON successfully and while booting, the below pint is displayed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-nxp/imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Nov 02 2020 - 12:48:26 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.1 69 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 55C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: i.MX6ULL iW-RAINBOW-G18M-SM&lt;BR /&gt;Boot Device: NAND&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=0&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=1&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202&lt;BR /&gt;wait_for_sr_state: failed sr=a2 cr=88 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x8 retry=2&lt;BR /&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x1d scl.gp=0x1c&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x21a0000&lt;BR /&gt;Can't find PMIC:PFUZE3000&lt;BR /&gt;initcall sequence 8ff91a8c failed at call 87804914 (err=-1)&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried resetting the board multiple times and observed same print.&lt;/P&gt;&lt;P&gt;One of the GPIO (E5 pin of CPU - CSI_PIXCLK) we are using for enabling peripheral power control for the switch. By default the GPIO is externally pulled down.&lt;/P&gt;&lt;P&gt;When the external pulldown is removed for the same GPIO, the board is successfully booting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly let me know what is the reason for such error when the pin is pulled down.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Nibin&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 06:59:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-Booting-error/m-p/1177722#M164497</guid>
      <dc:creator>NibinDasS</dc:creator>
      <dc:date>2020-11-04T06:59:10Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ULL Booting error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-Booting-error/m-p/1177845#M164503</link>
      <description>&lt;P&gt;Hi Nibin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;by default CSI_PIXCLK E5 pin is input with keeper as described in&lt;/P&gt;
&lt;P&gt;Table 91. 14 x 14 mm Functional Contact Assignments&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/docs/en/data-sheet/IMX6ULLIEC.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processors for Industrial Products&lt;/STRONG&gt;&lt;/A&gt;&amp;nbsp;, so you can check&lt;/P&gt;
&lt;P&gt;suitable for pmic level with oscillocope and set external pull resistor appropriately.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 09:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-Booting-error/m-p/1177845#M164503</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-04T09:43:09Z</dc:date>
    </item>
  </channel>
</rss>