<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 integrating touchscreen in kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/integrating-touchscreen-in-kernel/m-p/1177668#M164487</link>
    <description>&lt;P&gt;I am using Goodix Touch driver with Android 9.0 and kernel 4+&lt;BR /&gt;I use pin 263 (GPIO4) as interrupt pin .&lt;BR /&gt;But I get the following error :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;gpio-4 (GTP INT IRQ): _gpiod_direction_output_raw: tried to set a GPIO tied to an IRQ as output&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I checked the pin is defined as input pin.So does this mean that some other driver is trying to use it as output pin. If yes how can I find this driver that is occupying the pin. I found an ads7428 driver in the device tree file occupying this pin and I disabled it . Other than that I can't find any other driver using the pin.&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ketki K.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Nov 2020 04:29:19 GMT</pubDate>
    <dc:creator>Ketki</dc:creator>
    <dc:date>2020-11-04T04:29:19Z</dc:date>
    <item>
      <title>integrating touchscreen in kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/integrating-touchscreen-in-kernel/m-p/1177668#M164487</link>
      <description>&lt;P&gt;I am using Goodix Touch driver with Android 9.0 and kernel 4+&lt;BR /&gt;I use pin 263 (GPIO4) as interrupt pin .&lt;BR /&gt;But I get the following error :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;gpio-4 (GTP INT IRQ): _gpiod_direction_output_raw: tried to set a GPIO tied to an IRQ as output&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I checked the pin is defined as input pin.So does this mean that some other driver is trying to use it as output pin. If yes how can I find this driver that is occupying the pin. I found an ads7428 driver in the device tree file occupying this pin and I disabled it . Other than that I can't find any other driver using the pin.&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ketki K.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 04:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/integrating-touchscreen-in-kernel/m-p/1177668#M164487</guid>
      <dc:creator>Ketki</dc:creator>
      <dc:date>2020-11-04T04:29:19Z</dc:date>
    </item>
    <item>
      <title>Re: integrating touchscreen in kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/integrating-touchscreen-in-kernel/m-p/1177848#M164504</link>
      <description>&lt;P&gt;Hi Ketki&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for debugging Goodix touch driver one can look at:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Device-tree-binding-can-not-make-work-my-touch-device/td-p/637667" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Device-tree-binding-can-not-make-work-my-touch-device/td-p/637667&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://titanwolf.org/Network/Articles/Article?AID=7ccfac10-bc61-4011-982d-db257f545ac1#gsc.tab=0" target="_blank"&gt;https://titanwolf.org/Network/Articles/Article?AID=7ccfac10-bc61-4011-982d-db257f545ac1#gsc.tab=0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 09:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/integrating-touchscreen-in-kernel/m-p/1177848#M164504</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-04T09:47:40Z</dc:date>
    </item>
  </channel>
</rss>