<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power over SDIO iM8MQ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176620#M164378</link>
    <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;Yes, I see that SD2_VSELECT is related to switching between 1.8 and 3.3 Volts, which basically connected to speed mode of SDIO communication - high speed or ultra-high-speed. I'm using the module which generally works only in UHS mode and it means that the host and module should use 1.8 V for SDIO signals.&lt;/P&gt;&lt;P&gt;However, that is not related to power rail on SD slot - VSD_3V3 - it should always be 3.3V which intended to supply external devices. Hence I see that especially it doesn't work for my case and somehow processor doesn't want to switch on the power.&lt;/P&gt;&lt;P&gt;Sorry for my ignorance, but I didn't find information about SD2_NRST and POR_B, could you please explain to me what is the working algorithm with which processor recognize SD device and send logic levels at these pins?&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Evgenii&lt;/P&gt;</description>
    <pubDate>Mon, 02 Nov 2020 11:29:17 GMT</pubDate>
    <dc:creator>evgenii_platono</dc:creator>
    <dc:date>2020-11-02T11:29:17Z</dc:date>
    <item>
      <title>Power over SDIO iM8MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176202#M164335</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question regarding the evaluation board with iMX8MQ. I would like to use one external Wifi module, which should be supplied over SDIO 3.3V from the host platform. When I plug in SD adapter which connects my Wifi module with iMX to appropriate SD slot, I've figured out that some seconds EVB supply my module with 3.3V, but after a small period of time it completely switches off the voltage rail.&lt;/P&gt;&lt;P&gt;From iMX8MQ-EVB schematic, I could see that there is a transistor Q1602, which is responsible for SDIO power and looks like that it disconnects power from the module. Moreover, I see two control signals which directly go to the processor - SD2_NRST and POR_B. Also, there is bypass resistor R1606 which allows simple supplying scheme without any logic signals. I soldered this resistor in and with this workaround the power goes well to my module.&lt;/P&gt;&lt;P&gt;Could I ask you kindly explain what is the reason why the processor switches off the power from SD slot? Also, could you clarify what are the signals SD2_NRST and POR_B and how they play role in such case?&lt;/P&gt;&lt;P&gt;Thank you very much in advance!&lt;/P&gt;</description>
      <pubDate>Sat, 31 Oct 2020 23:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176202#M164335</guid>
      <dc:creator>evgenii_platono</dc:creator>
      <dc:date>2020-10-31T23:59:21Z</dc:date>
    </item>
    <item>
      <title>Re: Power over SDIO iM8MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176283#M164344</link>
      <description>&lt;P&gt;Hi evgenii_platono&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt; reason why the processor switches off the power from SD slot&lt;/P&gt;
&lt;P&gt;transistor Q1602 is depicted on schematic p.19 "SD3.0 PWR", NVCC_SD2 may be 1.8V/3.3V as described &lt;BR /&gt;on p.19, SD2_VSELECT. This is required by voltage swithching to 1.8V signaling mode, &lt;BR /&gt;voltage switching sequence is described in SD 3.0 specification. &lt;BR /&gt;SD2_NRST and POR_B are used as "power cycle" signals and also described in SD 3.0 specification.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 00:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176283#M164344</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-02T00:12:42Z</dc:date>
    </item>
    <item>
      <title>Re: Power over SDIO iM8MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176620#M164378</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;Yes, I see that SD2_VSELECT is related to switching between 1.8 and 3.3 Volts, which basically connected to speed mode of SDIO communication - high speed or ultra-high-speed. I'm using the module which generally works only in UHS mode and it means that the host and module should use 1.8 V for SDIO signals.&lt;/P&gt;&lt;P&gt;However, that is not related to power rail on SD slot - VSD_3V3 - it should always be 3.3V which intended to supply external devices. Hence I see that especially it doesn't work for my case and somehow processor doesn't want to switch on the power.&lt;/P&gt;&lt;P&gt;Sorry for my ignorance, but I didn't find information about SD2_NRST and POR_B, could you please explain to me what is the working algorithm with which processor recognize SD device and send logic levels at these pins?&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Evgenii&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 11:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176620#M164378</guid>
      <dc:creator>evgenii_platono</dc:creator>
      <dc:date>2020-11-02T11:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: Power over SDIO iM8MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176707#M164389</link>
      <description>&lt;P&gt;&amp;gt;VSD_3V3 - it should always be 3.3V which intended to supply external devices.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;during switching to 1.8v signaling mode it may be turned off for a short time.&lt;/P&gt;
&lt;P&gt;Suggest to check signals with logic analyzer and verify them with SD 3.0 specification.&lt;/P&gt;
&lt;P&gt;Also reason may be that SD port can not provide sufficient current to wifi module,&lt;/P&gt;
&lt;P&gt;one can try external power supply.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-over-SDIO-iM8MQ/m-p/1176707#M164389</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-02T14:42:02Z</dc:date>
    </item>
  </channel>
</rss>