<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which development board for 4 camera capture using MIPI?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227269#M16414</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Weidong Sun:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;您好，請問一下您有ADV7280-M對i.mx6 我們目前接 進I.MX6的PIN, 請問有這部份driver嗎?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVCC_MIPI :&lt;/P&gt;&lt;P&gt;CSI_CLK0M&lt;/P&gt;&lt;P&gt;CSI_CLK0P&lt;/P&gt;&lt;P&gt;CSI_D0M&lt;/P&gt;&lt;P&gt;CSI_D0P&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:darren_wang@compal.com"&gt;darren_wang@compal.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Sep 2014 02:32:19 GMT</pubDate>
    <dc:creator>darrenwang</dc:creator>
    <dc:date>2014-09-04T02:32:19Z</dc:date>
    <item>
      <title>Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227262#M16407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to record 4 analog camera's using a i.MX6 mpu to a SD card for analytic. The idea is that I use the MIPI port of the MX6 for the camera's. To convert the analog signal to MIPI CSI I want to use the ADV7820M chip. question one: is this possible? and question 2.&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I have 2 boards to choose from:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RioTBoard: uses a i.MX6 SOLO MPU or the MARS board which uses a i.MX6 Dual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Money wise I would pick the RiotBoard as this has a lower price-point, but I want to know if it even possible to capture 4 camera's this way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;Okay, I looked around some more... The SOLO has only 2 data lanes so that ain't gonna cut it but the DUal does have 4 data lanes (800Mbit). So yea, I thought I will use the Mars board.. Well there is no MIPI connection on the board, and in the schematic of the board they weren't connected. Now I am considering the i.MX6 SABRELITE. Is this going to work with the ADV7280M?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2014 11:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227262#M16407</guid>
      <dc:creator>tostikoning</dc:creator>
      <dc:date>2014-02-12T11:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227263#M16408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Maarten,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;gt;&amp;gt;Now I am considering the i.MX6 SABRELITE. Is this going to work with the ADV7280M?&lt;BR /&gt;(1)Yes, it is.&lt;/P&gt;&lt;P&gt;On i.MX6 SABRELITE board, MIPI connector is reserved for customer's expansion.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42701i4270E6C3C9ABB296/image-size/large?v=v2&amp;amp;px=999" title="mipi-sabrelite.png" alt="mipi-sabrelite.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(2)Supporting ADV7280-M&lt;/P&gt;&lt;P&gt;On our sabreAI board, reserved a connetor for ADV7280M board,too. linux and android bsp both support ADV7280M.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42702iC9C60DBEEDCD9049/image-size/large?v=v2&amp;amp;px=999" title="mipi-7280.png" alt="mipi-7280.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so you can use Sabrelite board and ADV7280M&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 03:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227263#M16408</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2014-02-13T03:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227264#M16409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So correct me if I'm wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can use the Linux BSP version for the i.MX6 series, which is like a Linux for the whole i.MX6 series and thus, also available for the SABRELITE board. In the Linux BSP is already a kernel present to decode 4 videostreams from the ADV7280M right? This would be perfect, as I only have to load the BSP on the board and connect a board with the ADV7280. It would be easy to record those streams to a SD card? I don't have any experience with these OS based boards. (I'm a microcontroller (cortexm0) kind of guy)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 07:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227264#M16409</guid>
      <dc:creator>tostikoning</dc:creator>
      <dc:date>2014-02-13T07:40:22Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227265#M16410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Maarten,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I checked the datasheet of adv7280, even if there are multi channel video input, It can only handle one channel at same time ! you had better confirm it with ADI . See MUX BLOCK in the following diagram.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42685i1116BD024E909104/image-size/large?v=v2&amp;amp;px=999" title="adv7280m.png" alt="adv7280m.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So maybe you can't use 4 channel video simutaneously.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 08:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227265#M16410</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2014-02-13T08:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227266#M16411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I come to the same conclusion when studying the ADV7280M Datasheet. I found the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42697iC55B1DDE3508CA43/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG.png" alt="Capture.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also the following: &lt;EM&gt;"The output of the ADV7280-M consists of a single data channel ..." &lt;/EM&gt;Which suggest it is only possible to decode a single input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Back to the drawing board...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 08:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227266#M16411</guid>
      <dc:creator>tostikoning</dc:creator>
      <dc:date>2014-02-13T08:24:35Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227267#M16412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Maarten,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We have a solution for multiple CVBS video input, It uses PCIe interface on i.mx6 to recieve digital video stream. you can refer to this address:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95143" style="background-color: #ffffff; text-indent: 0px; color: #1e5494; text-decoration: underline;" target="_blank"&gt;https://community.freescale.com/docs/DOC-95143&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 08:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227267#M16412</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2014-02-13T08:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227268#M16413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I will consider that option. Maybe I will go for the Toshiba chip metioned in a different thread: &lt;A href="http://www.toshiba.com/taec/components/ProdBrief/11J02_TC358746_ProdBrief.pdf" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #6a737b;" title="http://www.toshiba.com/taec/components/ProdBrief/11J02_TC358746_ProdBrief.pdf"&gt;http://www.toshiba.com/taec/components/ProdBrief/11J02_TC358746_ProdBrief.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 10:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227268#M16413</guid>
      <dc:creator>tostikoning</dc:creator>
      <dc:date>2014-02-13T10:16:44Z</dc:date>
    </item>
    <item>
      <title>Re: Which development board for 4 camera capture using MIPI?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227269#M16414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Weidong Sun:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;您好，請問一下您有ADV7280-M對i.mx6 我們目前接 進I.MX6的PIN, 請問有這部份driver嗎?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVCC_MIPI :&lt;/P&gt;&lt;P&gt;CSI_CLK0M&lt;/P&gt;&lt;P&gt;CSI_CLK0P&lt;/P&gt;&lt;P&gt;CSI_D0M&lt;/P&gt;&lt;P&gt;CSI_D0P&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:darren_wang@compal.com"&gt;darren_wang@compal.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Sep 2014 02:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-development-board-for-4-camera-capture-using-MIPI/m-p/227269#M16414</guid>
      <dc:creator>darrenwang</dc:creator>
      <dc:date>2014-09-04T02:32:19Z</dc:date>
    </item>
  </channel>
</rss>