<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error opening /dev/fb0 on i.Mx8QXP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1173785#M164102</link>
    <description>&lt;P&gt;Hello Missed to add below changes also in above message,&lt;BR /&gt;&lt;BR /&gt;I have also commented the Reset PIN in DTS:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Kernel DTS File&lt;/STRONG&gt;: arch/arm64/boot/dts/freescale/imx8x-mek.dtsi&lt;BR /&gt;&lt;STRONG&gt;Chantes:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;lvds_bridge0: lvds-to-hdmi-bridge@4c {&lt;BR /&gt;compatible = "ite,it6263";&lt;BR /&gt;reg = &amp;lt;0x4c&amp;gt;;&lt;BR /&gt;//reset-gpios = &amp;lt;&amp;amp;pca9557_a 6 GPIO_ACTIVE_LOW&amp;gt;;&lt;/P&gt;&lt;P&gt;port {&lt;BR /&gt;it6263_0_in: endpoint {&lt;BR /&gt;remote-endpoint = &amp;lt;&amp;amp;lvds0_out&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Kailas K.&lt;/P&gt;</description>
    <pubDate>Tue, 27 Oct 2020 10:55:53 GMT</pubDate>
    <dc:creator>kailas_kharse</dc:creator>
    <dc:date>2020-10-27T10:55:53Z</dc:date>
    <item>
      <title>Error opening /dev/fb0 on i.Mx8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1173766#M164099</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We are using &lt;STRONG&gt;i.Mx8QXP C0&lt;/STRONG&gt; Custom Board, we are only using the Flex-SPI interface and LVDS0 Interface along with eMMC Card. We don't have any other peripheral on our board, we have leaveraged the design from i.MX8QXP MEK Baord. Following are the changes w.r.t. MEK.&lt;/P&gt;&lt;P&gt;1.Changing mini-SAS connector to Horizontal part&lt;BR /&gt;2.Removing voltage translator U203,&lt;BR /&gt;3.Adding pullup to MIPI_DSI0_EN (J1.A11 pin)&lt;BR /&gt;4.Removing 12V power to connector, changing power rails as per load switch.&lt;/P&gt;&lt;P&gt;We are using "&lt;STRONG&gt;imx-yocto-L5.4.24_2.1.0&lt;/STRONG&gt;" Yocto Build, I am alble to get the display in u-boot by following modifications.&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;U-Bo&lt;FONT size="4"&gt;ot:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&lt;STRONG&gt;File&lt;/STRONG&gt;: /arch/arm/dt&lt;/FONT&gt;s/fsl-imx8qxp-mek.dts&lt;BR /&gt;&lt;STRONG&gt;Changes&lt;/STRONG&gt;:&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;EM&gt;lvds-to-hdmi-bridge@4c {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;compatible = "ite,it6263";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;reg = &amp;lt;0x4c&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- reset-gpios = &amp;lt;&amp;amp;pca9557_a 6 GPIO_ACTIVE_LOW&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;+ /*reset-gpios = &amp;lt;&amp;amp;pca9557_a 6 GPIO_ACTIVE_LOW&amp;gt;;*/&lt;/EM&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Just by commenting the reset gpio, we are able to get the splash screen in U-boot. But I have also done the following changes in Kernel DTS files as below for LVDS.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Kernel DTS File&lt;/STRONG&gt;: arch/arm64/boot/dts/freescale/imx8x-mek.dtsi&lt;BR /&gt;&lt;STRONG&gt;Chantes:&lt;/STRONG&gt;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;FONT size="3"&gt;pinctrl_i2c0_mipi_lvds0: mipi_lvds0_i2c0_grp {&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;fsl,pins = &amp;lt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX8QXP_MIPI_DSI0_I2C0_SCL_MIPI_DSI0_I2C0_SCL 0xc6000020&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX8QXP_MIPI_DSI0_I2C0_SDA_MIPI_DSI0_I2C0_SDA 0xc6000020&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX8QXP_MIPI_DSI0_GPIO0_01_LSIO_GPIO1_IO28 0x00000020&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*IMX8QXP_MIPI_DSI0_GPIO0_01_LSIO_GPIO1_IO28 0x00000020*/&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;};&lt;/FONT&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;Also I have verified that all the config required for LVDS, LDB, FB, are present and enabled.&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Still I am getting the below error: (Boot Logs Snippet)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;P&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.475066] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.486216] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.502236] dpu-core 56180000.dpu: driver probed&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.508739] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.515390] [drm] No driver support for vblank timestamp query.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.521402] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.529878] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.537478] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.545034] imx-drm display-subsystem: failed to bind bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops): -517&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.555018] imx-drm display-subsystem: master bind failed: -517&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.828314] i2c i2c-20: LPI2C adapter registered&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.834131] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.840765] [drm] No driver support for vblank timestamp query.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.846771] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.855056] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.862443] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.869989] imx-drm display-subsystem: failed to bind bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops): -517&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" face="arial,helvetica,sans-serif"&gt;[ 5.879983] imx-drm display-subsystem: master bind failed: -517&lt;/FONT&gt;&lt;/P&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On Debug console when I use "&lt;STRONG&gt;psplash&lt;/STRONG&gt;" command I am getting "&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;Error Operning /dev/fb0&lt;/STRONG&gt;&lt;/FONT&gt;"&lt;/P&gt;&lt;P&gt;Can you please suggest tell that what are the changes needed to resolve this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Kailas K.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 10:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1173766#M164099</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2020-10-27T10:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error opening /dev/fb0 on i.Mx8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1173785#M164102</link>
      <description>&lt;P&gt;Hello Missed to add below changes also in above message,&lt;BR /&gt;&lt;BR /&gt;I have also commented the Reset PIN in DTS:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Kernel DTS File&lt;/STRONG&gt;: arch/arm64/boot/dts/freescale/imx8x-mek.dtsi&lt;BR /&gt;&lt;STRONG&gt;Chantes:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;lvds_bridge0: lvds-to-hdmi-bridge@4c {&lt;BR /&gt;compatible = "ite,it6263";&lt;BR /&gt;reg = &amp;lt;0x4c&amp;gt;;&lt;BR /&gt;//reset-gpios = &amp;lt;&amp;amp;pca9557_a 6 GPIO_ACTIVE_LOW&amp;gt;;&lt;/P&gt;&lt;P&gt;port {&lt;BR /&gt;it6263_0_in: endpoint {&lt;BR /&gt;remote-endpoint = &amp;lt;&amp;amp;lvds0_out&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Kailas K.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 10:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1173785#M164102</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2020-10-27T10:55:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error opening /dev/fb0 on i.Mx8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1174142#M164126</link>
      <description>&lt;P&gt;Hi Kailas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for "Error opening /dev/fb0" one can consider sect.6.2.2 Frame Buffer&amp;nbsp; &lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank" rel="noopener"&gt;i.MX Linux Reference Manual​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;"Frame buffer drivers are supported for i.MX 6 and i.MX 7 but not for i.MX 8."&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 01:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1174142#M164126</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-10-28T01:29:32Z</dc:date>
    </item>
    <item>
      <title>Re: Error opening /dev/fb0 on i.Mx8QXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1174210#M164135</link>
      <description>&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am able to get the display on i.Mx8QXP MEK Baord, but I am facing issue on custom board with the only above changes mentioned. In MEK is am able to get /dev/fb0 but for custom board I am facing issue.&lt;/P&gt;&lt;P&gt;Can you please tell what are the things required to be considered?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Kailas K.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 04:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-opening-dev-fb0-on-i-Mx8QXP/m-p/1174210#M164135</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2020-10-28T04:40:04Z</dc:date>
    </item>
  </channel>
</rss>