<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: BT HFP workflow for buses</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1173379#M164055</link>
    <description>&lt;P&gt;You need to review in the schematics of the board that you are using which channel of the PCM of the Bluetooth it is use in order to configure in ALSA the workflow that maybe selected.&lt;/P&gt;
&lt;P&gt;By default in our boards we only configure the codec to be the input and output, since Bluetooth it is not in our hardware board, it is externally added, like a module that need to be handle as an external audio board and in the configuration of Gstreamer or ALSA select the proper channel to get the HFP working&lt;/P&gt;
&lt;P&gt;You may contact the Bluetooth manufacturer or the Bluetooth module in order to see if the option it is available.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Oct 2020 22:23:17 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2020-10-26T22:23:17Z</dc:date>
    <item>
      <title>BT HFP workflow for buses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1170647#M163767</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please provide the document for BT HFP workflow for Android 9 Automotive to IMX8 board.&lt;/P&gt;&lt;P&gt;By default alsa uses the &lt;STRONG&gt;audio_policy_configuration_car.xml . &lt;/STRONG&gt;As per this configuration input device is mic and output device is bus0 or bus1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 03:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1170647#M163767</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2020-10-21T03:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: BT HFP workflow for buses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1172658#M163991</link>
      <description>&lt;P&gt;Why HFP voice is not getting from WM8960 (bus1_system_media_out)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Sat, 24 Oct 2020 06:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1172658#M163991</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2020-10-24T06:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: BT HFP workflow for buses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1173379#M164055</link>
      <description>&lt;P&gt;You need to review in the schematics of the board that you are using which channel of the PCM of the Bluetooth it is use in order to configure in ALSA the workflow that maybe selected.&lt;/P&gt;
&lt;P&gt;By default in our boards we only configure the codec to be the input and output, since Bluetooth it is not in our hardware board, it is externally added, like a module that need to be handle as an external audio board and in the configuration of Gstreamer or ALSA select the proper channel to get the HFP working&lt;/P&gt;
&lt;P&gt;You may contact the Bluetooth manufacturer or the Bluetooth module in order to see if the option it is available.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 22:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1173379#M164055</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2020-10-26T22:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: BT HFP workflow for buses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1173565#M164067</link>
      <description>&lt;P&gt;Thank you &lt;SPAN class="UserName lia-user-name lia-user-rank-NXP-TechSupport lia-component-message-view-widget-author-username"&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/10885" target="_self"&gt;&lt;SPAN class=""&gt;jamesbone&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sure I will check with vendor also.&lt;/P&gt;&lt;P&gt;Is it possible please share the HFP working log. It's good for debugging more.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 05:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT-HFP-workflow-for-buses/m-p/1173565#M164067</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2020-10-27T05:45:36Z</dc:date>
    </item>
  </channel>
</rss>