<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Where does the SDK set VBAR?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227209#M16403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tyler,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I understand you are using U-Boot to load the sdk right? If so, that is why the VBAR contains the last value of U-Boot. &lt;/P&gt;&lt;P&gt;If you see, you do not need U-Boot, you can create a SD bootable card with the SDK as boot image. &lt;/P&gt;&lt;P&gt;You can find this in the README.pdf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Dec 2013 17:40:05 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2013-12-13T17:40:05Z</dc:date>
    <item>
      <title>Where does the SDK set VBAR?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227205#M16399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm wondering where the Platform SDK sets up the Secure VBAR and vector table so that an interrupt causes a jump to the correct handler.&amp;nbsp; I'm using a debugger to load the SDK .elf on top of uboot and finding that the old uboot value is still sitting in the VBAR.&amp;nbsp; Is that part of the code missing in the SDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2013 23:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227205#M16399</guid>
      <dc:creator>shefft</dc:creator>
      <dc:date>2013-11-25T23:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Where does the SDK set VBAR?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227206#M16400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The answer is that it doesn't, and the code IS missing.&amp;nbsp; You have to add that yourself.&amp;nbsp; So nice that this omission was documented somewhere.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 16:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227206#M16400</guid>
      <dc:creator>shefft</dc:creator>
      <dc:date>2013-12-04T16:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: Where does the SDK set VBAR?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227207#M16401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tyler,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delay. I have checked and I found that the vector table is copied to&amp;nbsp; address 0x0093FFB8. &lt;/P&gt;&lt;P&gt;You can get this address from the linker file. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; .ram_vectors (ORIGIN(OCRAM) + LENGTH(OCRAM) - RAM_VECTORS_SIZE) (NOLOAD) :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __ram_vectors_start = .;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; . += RAM_VECTORS_SIZE;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __ram_vectors_end = .;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;gt; OCRAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if you see section 8.4.5 Exception Handling&amp;nbsp; in RM you can see that this address correponds to the address of the RAM exception table after and in the boot process. This would mean that the Boot ROM changes the VBAR and I assume that&amp;nbsp; maybe that is why the VBAR register never changes in the SDK. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2013 00:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227207#M16401</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2013-12-10T00:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: Where does the SDK set VBAR?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227208#M16402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, I actually had a different question though - I was wondering about the location in the code, not the location in memory.&amp;nbsp; I was able to apply a fix.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2013 20:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227208#M16402</guid>
      <dc:creator>shefft</dc:creator>
      <dc:date>2013-12-11T20:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: Where does the SDK set VBAR?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227209#M16403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tyler,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I understand you are using U-Boot to load the sdk right? If so, that is why the VBAR contains the last value of U-Boot. &lt;/P&gt;&lt;P&gt;If you see, you do not need U-Boot, you can create a SD bootable card with the SDK as boot image. &lt;/P&gt;&lt;P&gt;You can find this in the README.pdf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2013 17:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-does-the-SDK-set-VBAR/m-p/227209#M16403</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2013-12-13T17:40:05Z</dc:date>
    </item>
  </channel>
</rss>