<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX53-START-R's FLT/5V blink and can not start up! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227203#M16397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your kindly support,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Our Hardware engineer measured the PCB according to your guide, as following.&lt;/P&gt;&lt;P&gt;1. Power Apply Adapter is ok, input voltage is 5.2v when it not connect to board.&lt;/P&gt;&lt;P&gt;2. When power adapter plugin the board, both C2 and Power supply pin are not good, the voltage shift from 0-3v dynamically , but never stable.&lt;/P&gt;&lt;P&gt;3. C217 and C7 is not good because 5v on board is not good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Our engineer just pulse power off pin about 5-10 seconds and the board become this situation suddenly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you have experiences on it before,&amp;nbsp; I saw the similar problem post on community before, but no answer yet,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/message/307599#307599" title="https://community.freescale.com/message/307599#307599"&gt;https://community.freescale.com/message/307599#307599&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Edison&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Mar 2013 02:42:05 GMT</pubDate>
    <dc:creator>edisonxu</dc:creator>
    <dc:date>2013-03-18T02:42:05Z</dc:date>
    <item>
      <title>IMX53-START-R's FLT/5V blink and can not start up!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227201#M16395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We got a IMX53-START-R board this morning, but the board can not work at all now (make us very sad because we do need this board to do verification).&amp;nbsp; When the board was power on, only FLT(red) and 5V(green) is lighted, but both of them are blinking and none of them are stay on stable status. The blink frequency is about 2 times per seconds. The DB9 serial port doesn't output any message when board power on. So can anybody tell me what's happening? the SD card (with ubuntu image) is broken or the power manager unit is bad now? Any suggest is appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edison&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 15:02:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227201#M16395</guid>
      <dc:creator>edisonxu</dc:creator>
      <dc:date>2013-03-15T15:02:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX53-START-R's FLT/5V blink and can not start up!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227202#M16396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Edison&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Don't worry ! Would you like to help me meause several voltage ?&lt;/P&gt;&lt;P&gt;(1) C2 position.&lt;/P&gt;&lt;P&gt;Measure it , to check&amp;nbsp; if 5V is ok.&lt;/P&gt;&lt;P&gt;(2) C217 position&lt;/P&gt;&lt;P&gt;Here should be 3.8V, If 3.8V is OK, Do (3)&lt;/P&gt;&lt;P&gt;(3) C7 position&lt;/P&gt;&lt;P&gt;Here should be 3.2V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After you mesure it ,tell me result ,please !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Mar 2013 01:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227202#M16396</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-03-16T01:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX53-START-R's FLT/5V blink and can not start up!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227203#M16397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your kindly support,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Our Hardware engineer measured the PCB according to your guide, as following.&lt;/P&gt;&lt;P&gt;1. Power Apply Adapter is ok, input voltage is 5.2v when it not connect to board.&lt;/P&gt;&lt;P&gt;2. When power adapter plugin the board, both C2 and Power supply pin are not good, the voltage shift from 0-3v dynamically , but never stable.&lt;/P&gt;&lt;P&gt;3. C217 and C7 is not good because 5v on board is not good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Our engineer just pulse power off pin about 5-10 seconds and the board become this situation suddenly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you have experiences on it before,&amp;nbsp; I saw the similar problem post on community before, but no answer yet,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/message/307599#307599" title="https://community.freescale.com/message/307599#307599"&gt;https://community.freescale.com/message/307599#307599&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Edison&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 02:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227203#M16397</guid>
      <dc:creator>edisonxu</dc:creator>
      <dc:date>2013-03-18T02:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX53-START-R's FLT/5V blink and can not start up!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227204#M16398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Edison,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.2V is too High. On i.mx53-START-R borad, There is a overvoltage protection circuit. If your input voltage is over 5.1V, internal circuits will be protected. So you must ensure the output of&amp;nbsp; adapter is 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 04:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-START-R-s-FLT-5V-blink-and-can-not-start-up/m-p/227204#M16398</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-03-18T04:05:19Z</dc:date>
    </item>
  </channel>
</rss>