<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Display both VGA and HDMI  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227172#M16369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I remember there is some setprop for dual display. Is there any difference when you set it (as I remember you are able to determinate with display will be first one, please, let me know if I´m missing something)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the same monitor to display both VGA and HDMI? Is there any change that the blank areas are caused by monitor configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I branched it to a new discussion because maybe someone else can add some light on this issue. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Mar 2013 13:52:34 GMT</pubDate>
    <dc:creator>daiane_angolini</dc:creator>
    <dc:date>2013-03-15T13:52:34Z</dc:date>
    <item>
      <title>Display both VGA and HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227171#M16368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried this bootargs of dual display-&lt;/P&gt;&lt;P&gt;setenv bootargs console=ttymxc0 init=/init androidboot.console=ttymxc0 video=mxcdi0fb:RGB24,1280x720M@60 hdmi video=mxcdi1fb:GBR24,VGA-SVGA di1_primary vga ip=none pmem=128M,64M fbmem=28M gpu_memory=128M vmalloc=576M&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got both VGA and HDMI displays but HDMI screen area is scaled down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I turned off VGA and HDMI. Then configured new resolution for HDMI and turned it ON.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo 1 &amp;gt;/sys/class/graphics/fb0/blank&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #vga off&lt;/P&gt;&lt;P&gt;echo 1 &amp;gt;/sys/class/graphics/fb1/blank&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #hdmi off&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# cat /sys/class/graphics/fb1/modes&lt;/P&gt;&lt;P&gt;S:1280x720p-50&lt;/P&gt;&lt;P&gt;S:720x576p-50&lt;/P&gt;&lt;P&gt;S:1920x1080p-50&lt;/P&gt;&lt;P&gt;S:640x480p-60&lt;/P&gt;&lt;P&gt;S:720x480p-60&lt;/P&gt;&lt;P&gt;S:1280x720p-60&lt;/P&gt;&lt;P&gt;S:1920x1080p-60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;# echo S:1280x720p-60 &amp;gt;/sys/class/graphics/fb1/mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;# cat /sys/class/graphics/fb1/mode&lt;/P&gt;&lt;P&gt;S:1280x720p-60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;# echo 0 &amp;gt;/sys/class/graphics/fb1/blank&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #hdmi on&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Still the hdmi is not using the entire display area. Both ends are left blank.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;.How can I make my HDMI display "FULLSCREEN"?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 04:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227171#M16368</guid>
      <dc:creator>Mats1z</dc:creator>
      <dc:date>2013-03-15T04:26:20Z</dc:date>
    </item>
    <item>
      <title>Re: Display both VGA and HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227172#M16369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I remember there is some setprop for dual display. Is there any difference when you set it (as I remember you are able to determinate with display will be first one, please, let me know if I´m missing something)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the same monitor to display both VGA and HDMI? Is there any change that the blank areas are caused by monitor configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I branched it to a new discussion because maybe someone else can add some light on this issue. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 13:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227172#M16369</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-03-15T13:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: Display both VGA and HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227173#M16370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;I'm using android 2.3 a.k.a gingerbread.&lt;/LI&gt;&lt;LI&gt;setprop rw.SECOND_DISPLAY_CONNECTED=1 , this is configured automatically when hdmi cable is connected.&lt;/LI&gt;&lt;LI&gt;if hdmi is configured as primary display there is no problem of display scaling but dynamic detection becomes impossible.&lt;/LI&gt;&lt;LI&gt;my setup works only when vga is primary display&amp;nbsp; and HDMI is secondary&lt;/LI&gt;&lt;LI&gt;I use 2 displays , one for vga and lcd for hdmi&lt;/LI&gt;&lt;LI&gt;when hdmi is primary display the entire screen area of display is used. So i don't think its an issue with monitor/lcd&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2013 04:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227173#M16370</guid>
      <dc:creator>Mats1z</dc:creator>
      <dc:date>2013-03-19T04:25:28Z</dc:date>
    </item>
    <item>
      <title>Re: Display both VGA and HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227174#M16371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Mats1z,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There only 1 IPU module in i.mx53 SOC, The biggest resolution is 1920x1080, If you want dual display by VGA and HDMI ports. Resolution should be suitable to be arragened.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please try :&lt;/P&gt;&lt;P&gt;VGA&amp;nbsp; : 1024x768&lt;/P&gt;&lt;P&gt;HDMI : 1024x768&lt;/P&gt;&lt;P&gt;Then check if image can display the entire screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2013 05:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-both-VGA-and-HDMI/m-p/227174#M16371</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-03-19T05:53:26Z</dc:date>
    </item>
  </channel>
</rss>