<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEncrypt a device by using CAAM on iMX7</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1169121#M163616</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to have a secure boot chain which will have the rootfs decryption integrated. The board would boot up to the initramfs, where I would like to decrypt the rootfs and mount it.The following requirement is to be fulfilled:&lt;/P&gt;&lt;P&gt;- the rootfs partition should be encrypted on the host machine in Yocto&lt;/P&gt;&lt;P&gt;I am not sure how to proceed with this. I have found the following two documents which describe how to create an encrypted storage by using the CAAM module:&lt;/P&gt;&lt;P&gt;- AN12554 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12554.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12554.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;- AN12714 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12714.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12714.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;As I can see, the latter document is newer (from February 2020) but seems like a device is encrypted on the target, which is not what I want. The former document is from August 2019 and seems to support the device encryption on the host and its decryption on the target.&lt;/P&gt;&lt;P&gt;Could someone assist me on how I should proceed on this?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aleksandar&lt;/P&gt;</description>
    <pubDate>Sat, 17 Oct 2020 10:09:50 GMT</pubDate>
    <dc:creator>aleksandar_niko</dc:creator>
    <dc:date>2020-10-17T10:09:50Z</dc:date>
    <item>
      <title>Encrypt a device by using CAAM on iMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1169121#M163616</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to have a secure boot chain which will have the rootfs decryption integrated. The board would boot up to the initramfs, where I would like to decrypt the rootfs and mount it.The following requirement is to be fulfilled:&lt;/P&gt;&lt;P&gt;- the rootfs partition should be encrypted on the host machine in Yocto&lt;/P&gt;&lt;P&gt;I am not sure how to proceed with this. I have found the following two documents which describe how to create an encrypted storage by using the CAAM module:&lt;/P&gt;&lt;P&gt;- AN12554 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12554.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12554.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;- AN12714 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12714.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12714.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;As I can see, the latter document is newer (from February 2020) but seems like a device is encrypted on the target, which is not what I want. The former document is from August 2019 and seems to support the device encryption on the host and its decryption on the target.&lt;/P&gt;&lt;P&gt;Could someone assist me on how I should proceed on this?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aleksandar&lt;/P&gt;</description>
      <pubDate>Sat, 17 Oct 2020 10:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1169121#M163616</guid>
      <dc:creator>aleksandar_niko</dc:creator>
      <dc:date>2020-10-17T10:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypt a device by using CAAM on iMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1170332#M163741</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/153013"&gt;@aleksandar_niko&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; We do not have example for Your situation. &lt;BR /&gt;You may use the recent NXP Linux BSP (L5.4.47). Look at section 9.5 (Disk &lt;BR /&gt;encryption acceleration) of "IMX_LINUX_USERS_GUIDE.pdf".&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 12:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1170332#M163741</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-10-20T12:01:32Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypt a device by using CAAM on iMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1186234#M165233</link>
      <description>&lt;P&gt;Thanks Yuri.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 21:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypt-a-device-by-using-CAAM-on-iMX7/m-p/1186234#M165233</guid>
      <dc:creator>aleksandar_niko</dc:creator>
      <dc:date>2020-11-19T21:05:05Z</dc:date>
    </item>
  </channel>
</rss>