<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to make the raspberry pi camera work with imx8mm in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1169116#M163614</link>
    <description>&lt;P&gt;To attach a camera module to a Pi Zero:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Remove the existing camera module’s cable by gently lifting the collar on the camera module and pulling the cable out.&lt;/LI&gt;&lt;LI&gt;Next, insert the wider end of the adapter cable with the conductors facing in the same direction as the camera’s lens.&lt;/LI&gt;&lt;LI&gt;Finally, attach the adapter to the Pi Zero by gently lifting the collar at the edge of the board (be careful with this as they are more delicate than the collars on the regular CSI ports) and inserting the smaller end of the adapter with the conductors facing the back of the Pi Zero.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;You will need to reboot after doing this (but this is one-time setup so you won’t need to do it again unless you re-install your operating system or switch SD cards). Once rebooted, start a terminal and try the following command:&lt;/P&gt;&lt;DIV class="highlight-bash notranslate"&gt;&lt;DIV class="highlight"&gt;&lt;PRE&gt;raspistill -o image.jpg&lt;/PRE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;If everything is working correctly, the camera should start, a preview from the camera should appear on the display and, after a 5 second delay it should capture an image (storing it as&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="pre"&gt;image.jpg&lt;/SPAN&gt;) before shutting down the camera.&lt;/P&gt;</description>
    <pubDate>Sat, 17 Oct 2020 09:01:59 GMT</pubDate>
    <dc:creator>Hermanl</dc:creator>
    <dc:date>2020-10-17T09:01:59Z</dc:date>
    <item>
      <title>How to make the raspberry pi camera work with imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1168906#M163586</link>
      <description>&lt;P&gt;I am working on an imx8mm evk board with a custom linux&amp;nbsp; bootloader and kernel. But the filesystem used is the same as the distributed version by nxp. I have previously made use of the MIMMINITOCSI camera by NXP for streaming and capturing images.&lt;/P&gt;&lt;P&gt;I use the following commands:&lt;/P&gt;&lt;P&gt;$ gst-launch-1.0 v4l2src num-buffers=1 &lt;SPAN class="pl-k"&gt;!&lt;/SPAN&gt; jpegenc &lt;SPAN class="pl-k"&gt;!&lt;/SPAN&gt; filesink location=/tmp/test.jpg&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;$ gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=1920,height=1080 ! waylandsink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use the imx8mm evk board and the raspberry pi camera to stream and capture images. When I use the commands above I get the following errors&lt;/P&gt;&lt;P&gt;$ gst-launch-1.0 v4l2src num-buffers=1 &lt;SPAN class="pl-k"&gt;!&lt;/SPAN&gt; jpegenc &lt;SPAN class="pl-k"&gt;!&lt;/SPAN&gt; filesink location=/tmp/test.jpg&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Pipeline is live and does not need PREROLL ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.&lt;BR /&gt;Additional debug info:&lt;BR /&gt;../../../../git/libs/gst/base/gstbasesrc.c(3072): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;BR /&gt;streaming stopped, reason not-negotiated (-4)&lt;BR /&gt;Execution ended after 0:00:00.000215875&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Setting pipeline to READY ...&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;and a similar one stating internal data stream error for the other command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could someone direct me towards how do I go about achieving this?&lt;/P&gt;</description>
      <pubDate>Fri, 16 Oct 2020 13:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1168906#M163586</guid>
      <dc:creator>anurag16doshi</dc:creator>
      <dc:date>2020-10-16T13:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to make the raspberry pi camera work with imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1169105#M163608</link>
      <description>&lt;P&gt;Hi anurag16doshi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this camera uses IMX219 sensor and one can try suggestions provided on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-New-MIPI-CSI-Camera-Driver-Integration/m-p/1161471#M162766" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-New-MIPI-CSI-Camera-Driver-Integration/m-p/1161471#M162766&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 17 Oct 2020 05:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1169105#M163608</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-10-17T05:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to make the raspberry pi camera work with imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1169116#M163614</link>
      <description>&lt;P&gt;To attach a camera module to a Pi Zero:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Remove the existing camera module’s cable by gently lifting the collar on the camera module and pulling the cable out.&lt;/LI&gt;&lt;LI&gt;Next, insert the wider end of the adapter cable with the conductors facing in the same direction as the camera’s lens.&lt;/LI&gt;&lt;LI&gt;Finally, attach the adapter to the Pi Zero by gently lifting the collar at the edge of the board (be careful with this as they are more delicate than the collars on the regular CSI ports) and inserting the smaller end of the adapter with the conductors facing the back of the Pi Zero.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;You will need to reboot after doing this (but this is one-time setup so you won’t need to do it again unless you re-install your operating system or switch SD cards). Once rebooted, start a terminal and try the following command:&lt;/P&gt;&lt;DIV class="highlight-bash notranslate"&gt;&lt;DIV class="highlight"&gt;&lt;PRE&gt;raspistill -o image.jpg&lt;/PRE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;If everything is working correctly, the camera should start, a preview from the camera should appear on the display and, after a 5 second delay it should capture an image (storing it as&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="pre"&gt;image.jpg&lt;/SPAN&gt;) before shutting down the camera.&lt;/P&gt;</description>
      <pubDate>Sat, 17 Oct 2020 09:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-the-raspberry-pi-camera-work-with-imx8mm/m-p/1169116#M163614</guid>
      <dc:creator>Hermanl</dc:creator>
      <dc:date>2020-10-17T09:01:59Z</dc:date>
    </item>
  </channel>
</rss>