<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CANBus interface for i.MX8QM MEK board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1168321#M163529</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My aim is to enable the CAN interface for the i.MX8QM MEK attached to the base board. I'm running Android 10 (imx-android-10.0.0_2.3.0). I can't find the CAN interface when I execute 'ifconfig -a'. I noticed that the base board supports CAN FD which I believe is not supported for Android. Is there a way to use the legacy CAN utilities? I've tried disabling CAN FD in the device tree as suggested &lt;A href="https://freescale.jiveon.com/message/1327851?commentID=1327851#comment-1327851" target="_self"&gt;here&lt;/A&gt;. However, I still haven't been able to view my CAN interfaces.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 15 Oct 2020 21:52:52 GMT</pubDate>
    <dc:creator>tpe</dc:creator>
    <dc:date>2020-10-15T21:52:52Z</dc:date>
    <item>
      <title>CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1168321#M163529</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My aim is to enable the CAN interface for the i.MX8QM MEK attached to the base board. I'm running Android 10 (imx-android-10.0.0_2.3.0). I can't find the CAN interface when I execute 'ifconfig -a'. I noticed that the base board supports CAN FD which I believe is not supported for Android. Is there a way to use the legacy CAN utilities? I've tried disabling CAN FD in the device tree as suggested &lt;A href="https://freescale.jiveon.com/message/1327851?commentID=1327851#comment-1327851" target="_self"&gt;here&lt;/A&gt;. However, I still haven't been able to view my CAN interfaces.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 15 Oct 2020 21:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1168321#M163529</guid>
      <dc:creator>tpe</dc:creator>
      <dc:date>2020-10-15T21:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1169857#M163687</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Do you use the M4? By default, SCFW assigns CAN resources to M4 app.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So if you use M4 and you don't need CAN on M4 partition, then you need to comment this line&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE));&lt;/P&gt;
&lt;P&gt;from&amp;nbsp;void board_system_config(sc_bool_t early, sc_rm_pt_t pt_boot), board.c of SCFW porting kit.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Ivan.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Oct 2020 21:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1169857#M163687</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-10-19T21:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1170449#M163750</link>
      <description>&lt;P&gt;Hello Ivan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your input! Unfortunately, your suggestion did not solve my issue. I'm still unable to bring up the CAN interface after removing CAN from the M4 partition. Do I need to allocate those resources for my A53 or my A72 partition?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;tpe&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 17:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1170449#M163750</guid>
      <dc:creator>tpe</dc:creator>
      <dc:date>2020-10-20T17:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171305#M163833</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If the SC_CAN_* was removed from M4 partition, by default, those resources should be moved to A partition.&lt;/P&gt;
&lt;P&gt;Can you please provide a boot log and the used dtsi/dts?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Ivan.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 20:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171305#M163833</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-10-21T20:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171323#M163834</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is my bootlog. I'm using the default imx8qm-mek.dts and imx8qm.dtsi files with the exception of disabling CAN FD for the three CAN devices. I noticed that my device tree FlexCAN configurations hold true for everything except the status was disabled. This is strange because when I decompiled the dtb, the status message was set to okay. I've also ran 'zcat proc/config.gz | grep CAN' to verify that FlexCAN was enabled by the kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 21:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171323#M163834</guid>
      <dc:creator>tpe</dc:creator>
      <dc:date>2020-10-21T21:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171974#M163912</link>
      <description>&lt;P&gt;I have solved this issue. The device tree blob includes imx8qm-mek-ov5640.dts which includes another device tree file called imx8qm-mek-rpmsg.dts that overrides the configurations for the FlexCAN and regulators' status to be disabled in imx8qm-mek.dts. I am relatively new to Android source code so it wasn't obvious for me to check the device tree files for camera display. Hopefully this helps anyone else who has this problem!&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 17:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1171974#M163912</guid>
      <dc:creator>tpe</dc:creator>
      <dc:date>2020-10-22T17:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1279788#M174332</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please add the link for disabling the CANFD in device tree again.&lt;/P&gt;&lt;P&gt;The link seems to be not working.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Preetam&lt;/P&gt;</description>
      <pubDate>Thu, 20 May 2021 13:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1279788#M174332</guid>
      <dc:creator>preetamch29</dc:creator>
      <dc:date>2021-05-20T13:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: CANBus interface for i.MX8QM MEK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1285962#M174880</link>
      <description>&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;I am also facing the same problem.&lt;/P&gt;&lt;P&gt;I have made the changes in board.c and generated scfw-tcm.bin and flash.bin. but I am unable to flash this ''flash.bin' to imx8qm. I am using "imx-android-11.0.0_1.0.0".&lt;/P&gt;&lt;P&gt;I am using following command to flash:&lt;/P&gt;&lt;P&gt;uuu -b emmc flash.bin flash.bin&lt;/P&gt;&lt;P&gt;How should I add this changed flash.bin or scfw.bin in my images?&lt;/P&gt;&lt;P&gt;my CAN interfaces gets diabled as shown below in bootup log:&lt;/P&gt;&lt;P&gt;Line 607: [ 4.439486] can01-stby: supplied by can01-en&lt;BR /&gt;Line 607: [ 4.439486] can01-stby: supplied by can01-en&lt;BR /&gt;Line 646: [ 5.437399] logwrapper: Cannot log to file /dev/fscklogs/log&lt;BR /&gt;Line 708: [ 7.413427] apexd: Scanning /system/apex for preinstalled data&lt;BR /&gt;Line 709: [ 7.425017] apexd: Scanning /system_ext/apex for preinstalled data&lt;BR /&gt;Line 711: [ 7.435821] apexd: Scanning /vendor/apex for preinstalled data&lt;BR /&gt;Line 713: [ 7.446248] apexd: Scanning /system/apex looking for APEX packages.&lt;BR /&gt;Line 756: [ 10.897623] apexd: Scanning /system/apex for preinstalled data&lt;BR /&gt;Line 757: [ 10.908377] apexd: Scanning /system_ext/apex for preinstalled data&lt;BR /&gt;Line 759: [ 10.919221] apexd: Scanning /product/apex for preinstalled data&lt;BR /&gt;Line 761: [ 10.929779] apexd: Scanning /vendor/apex for preinstalled data&lt;BR /&gt;Line 821: [ 19.285285] apexd: Can't open /system_ext/apex for reading : No such file or directory&lt;BR /&gt;Line 822: [ 19.293286] apexd: Can't open /product/apex for reading : No such file or directory&lt;BR /&gt;Line 823: [ 19.301101] apexd: Can't open /vendor/apex for reading : No such file or directory&lt;BR /&gt;Line 863: [ 35.905126] can01-en: disabling&lt;BR /&gt;Line 864: [ 35.908363] can01-stby: disabling&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 07:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CANBus-interface-for-i-MX8QM-MEK-board/m-p/1285962#M174880</guid>
      <dc:creator>preetamch29</dc:creator>
      <dc:date>2021-06-02T07:59:49Z</dc:date>
    </item>
  </channel>
</rss>