<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 USB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1167861#M163485</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;DIV class="container"&gt;&lt;DIV class="frame"&gt;&lt;DIV class="page tlid-homepage homepage translate-text"&gt;&lt;DIV class="homepage-content-wrap"&gt;&lt;DIV class="tlid-source-target main-header"&gt;&lt;DIV class="source-target-row"&gt;&lt;DIV class="tlid-results-container results-container"&gt;&lt;DIV class="tlid-result result-dict-wrapper"&gt;&lt;DIV class="result tlid-copy-target"&gt;&lt;DIV class="text-wrap tlid-copy-target"&gt;&lt;DIV class="result-shield-container tlid-copy-target"&gt;&lt;SPAN class="tlid-translation translation"&gt;&lt;SPAN&gt;Is there any problem with the following wiring?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="result-shield-container tlid-copy-target"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;gt;1. USB LDO should have input&lt;BR /&gt;&amp;gt;USB OTG1 VBUS&amp;nbsp;&lt;/P&gt;&lt;P&gt;→(5V USB connector input)&lt;/P&gt;&lt;P&gt;&amp;gt;2. USB OTG1 ID pin should be pulled up to High via 10K resistor.&lt;BR /&gt;&amp;gt;USB OTG1 ID's level determines USB OTG1 work mode(device or host)&lt;/P&gt;&lt;P&gt;i.MX6 （device） 　USB OTG1 ID : 10kΩ　3.3V pull -up ？　&lt;/P&gt;&lt;P&gt;3. GND pin&lt;/P&gt;&lt;P&gt;GND&lt;/P&gt;&lt;P&gt;Best Regard&lt;/P&gt;</description>
    <pubDate>Thu, 15 Oct 2020 01:24:49 GMT</pubDate>
    <dc:creator>ban45</dc:creator>
    <dc:date>2020-10-15T01:24:49Z</dc:date>
    <item>
      <title>i.MX6 USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1160959#M162712</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;When using i.MX6 ULL on the USB device side&lt;BR /&gt;Is it okay to connect only the DP and DN terminals?&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 01:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1160959#M162712</guid>
      <dc:creator>ban45</dc:creator>
      <dc:date>2020-09-30T01:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1161013#M162716</link>
      <description>&lt;P&gt;Hi Ban45,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;Is it okay to connect only the DP and DN terminals?&lt;BR /&gt;Yes. But the following conditions should be met:&lt;BR /&gt;1. USB LDO should have input&lt;BR /&gt;Internal USB LDO has 2 input powers:&lt;BR /&gt;---USB OTG1 VBUS &amp;amp; USB OTG2 VBUS&lt;BR /&gt;USB LDO will select one of them to be input, so you should ensure one of them to be 5V Power.&lt;BR /&gt;Because USB LDO supplies 2 USB PHYs.&lt;/P&gt;
&lt;P&gt;2. USB OTG1 ID pin should be pulled up to High via 10K resistor.&lt;BR /&gt;USB OTG1 ID's level determines USB OTG1 work mode(device or host)&lt;/P&gt;
&lt;P&gt;3. GND pin&lt;BR /&gt;If you want to connect the USB port to external device(Not on board), GND pin should be needed.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Test it on your board, please!&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 03:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1161013#M162716</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-09-30T03:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1167861#M163485</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;DIV class="container"&gt;&lt;DIV class="frame"&gt;&lt;DIV class="page tlid-homepage homepage translate-text"&gt;&lt;DIV class="homepage-content-wrap"&gt;&lt;DIV class="tlid-source-target main-header"&gt;&lt;DIV class="source-target-row"&gt;&lt;DIV class="tlid-results-container results-container"&gt;&lt;DIV class="tlid-result result-dict-wrapper"&gt;&lt;DIV class="result tlid-copy-target"&gt;&lt;DIV class="text-wrap tlid-copy-target"&gt;&lt;DIV class="result-shield-container tlid-copy-target"&gt;&lt;SPAN class="tlid-translation translation"&gt;&lt;SPAN&gt;Is there any problem with the following wiring?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="result-shield-container tlid-copy-target"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;gt;1. USB LDO should have input&lt;BR /&gt;&amp;gt;USB OTG1 VBUS&amp;nbsp;&lt;/P&gt;&lt;P&gt;→(5V USB connector input)&lt;/P&gt;&lt;P&gt;&amp;gt;2. USB OTG1 ID pin should be pulled up to High via 10K resistor.&lt;BR /&gt;&amp;gt;USB OTG1 ID's level determines USB OTG1 work mode(device or host)&lt;/P&gt;&lt;P&gt;i.MX6 （device） 　USB OTG1 ID : 10kΩ　3.3V pull -up ？　&lt;/P&gt;&lt;P&gt;3. GND pin&lt;/P&gt;&lt;P&gt;GND&lt;/P&gt;&lt;P&gt;Best Regard&lt;/P&gt;</description>
      <pubDate>Thu, 15 Oct 2020 01:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB/m-p/1167861#M163485</guid>
      <dc:creator>ban45</dc:creator>
      <dc:date>2020-10-15T01:24:49Z</dc:date>
    </item>
  </channel>
</rss>