<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6DQ IPU CPMEM Bus Address in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1167106#M163435</link>
    <description>&lt;P&gt;Found the answer in Section 37.4.2.10.2 of the RM. Although each mega-word is 160 bits (5x 32-bit words), each word has to start on a 256-bit boundary (8x 32-bit words).&lt;/P&gt;&lt;P&gt;Thanks for your quick response.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Oct 2020 04:26:39 GMT</pubDate>
    <dc:creator>ogj</dc:creator>
    <dc:date>2020-10-14T04:26:39Z</dc:date>
    <item>
      <title>iMX6DQ IPU CPMEM Bus Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1166952#M163422</link>
      <description>&lt;P&gt;I'd like to know the bus address for the CPMEM for ipu1 and ipu2 in the iMX6Q. According to the RM, ipu1 is at 0x0260_0000 and ipu2 is at 0x02A0_0000. It appears from the SDK that the CPMEM is at the ipu base address + 0x0010_0000, but I'd like to make sure.&lt;/P&gt;&lt;P&gt;Another thing that puzzles me is the the RM shows the structure of the CPMEM as 80 channels x 2 mega-words per channel; each mega-word being 160-bits (5x 32-bit words).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ogj_0-1602620976807.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127358i07B27CF0CC48EA54/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ogj_0-1602620976807.png" alt="ogj_0-1602620976807.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The SDK structs for the CPMEM are:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;struct ipu_cpmem_word&lt;BR /&gt;{&lt;BR /&gt;uint32_t data[5];&lt;BR /&gt;uint32_t res[3];&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;typedef struct ipu_cpmem&lt;BR /&gt;{&lt;BR /&gt;struct ipu_cpmem_word word[2];&lt;BR /&gt;} ipu_cpmem_t;&lt;/P&gt;&lt;P&gt;in the ipu_common.h file. I don't understand what the res[3] is for after each 160-bit mega-word.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;iMX6 SDK shows the structure of&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 20:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1166952#M163422</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-10-13T20:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DQ IPU CPMEM Bus Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1167012#M163427</link>
      <description>&lt;P&gt;Hi ogj&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;appears from the SDK that the CPMEM is at the ipu base address + 0x0010_0000,&lt;/P&gt;
&lt;P&gt;&amp;gt;but I'd like to make sure.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;correct&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;I don't understand what the res[3] is for after each 160-bit mega-word.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can refer to (Word 1) Table 37-14. Channel Parameters Memory&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX6DQRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 01:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1167012#M163427</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-10-14T01:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DQ IPU CPMEM Bus Address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1167106#M163435</link>
      <description>&lt;P&gt;Found the answer in Section 37.4.2.10.2 of the RM. Although each mega-word is 160 bits (5x 32-bit words), each word has to start on a 256-bit boundary (8x 32-bit words).&lt;/P&gt;&lt;P&gt;Thanks for your quick response.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 04:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-IPU-CPMEM-Bus-Address/m-p/1167106#M163435</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-10-14T04:26:39Z</dc:date>
    </item>
  </channel>
</rss>