<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.MX8M SPI device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-SPI-device/m-p/1166485#M163371</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using I.MX8MQ EVK and will development custom product.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have a plan to use a spi device. Currently, we are operating with androidoreo. Do we just need to modify the dts file? And I wonder how to modify it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;One more rudimentary question is, if the above processes are successful and the spi device is connected after the boot (assuming you've even raised the device driver), how can I confirm the connection?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you can give me any information, please reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Oct 2020 05:32:58 GMT</pubDate>
    <dc:creator>pjw</dc:creator>
    <dc:date>2020-10-13T05:32:58Z</dc:date>
    <item>
      <title>I.MX8M SPI device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-SPI-device/m-p/1166485#M163371</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using I.MX8MQ EVK and will development custom product.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have a plan to use a spi device. Currently, we are operating with androidoreo. Do we just need to modify the dts file? And I wonder how to modify it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;One more rudimentary question is, if the above processes are successful and the spi device is connected after the boot (assuming you've even raised the device driver), how can I confirm the connection?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you can give me any information, please reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 05:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-SPI-device/m-p/1166485#M163371</guid>
      <dc:creator>pjw</dc:creator>
      <dc:date>2020-10-13T05:32:58Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8M SPI device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-SPI-device/m-p/1166602#M163386</link>
      <description>&lt;P&gt;Hi pjw&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for using spi device one can add driver for it using linux guidelines and rules&lt;/P&gt;
&lt;P&gt;as android is based on linux. In particular one can look at sect.3.8 SPI NOR Flash&lt;/P&gt;
&lt;P&gt;Memory Technology Device (MTD), sect.3.8.5 Menu Configuration Options&lt;/P&gt;
&lt;P&gt;&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank" rel="noopener"&gt;i.MX Linux Reference Manual​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;for testing use unit test:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spi_test?h=imx_5.4.24_2.1.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spi_test?h=imx_5.4.24_2.1.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 08:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8M-SPI-device/m-p/1166602#M163386</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-10-13T08:33:31Z</dc:date>
    </item>
  </channel>
</rss>