<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX8M Mini cpufreq error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/1165933#M163299</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi Igor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have the same problem, but the point is our CPU is a commercial&amp;nbsp;i.MX8MMQ rev1.0 1800 MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is the problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Mon, 12 Oct 2020 08:18:17 GMT</pubDate>
    <dc:creator>wang_david-yb</dc:creator>
    <dc:date>2020-10-12T08:18:17Z</dc:date>
    <item>
      <title>i.MX8M Mini cpufreq error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996672#M147855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer i.MX8M Mini board shows serveral cpufreq error like below then hang.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;What may cause this error?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;[ 12.363180] cpu cpu0: failed to scale arm_reg up: -11&lt;BR /&gt;[ 12.368264] cpufreq: __target_index: Failed to change cpu frequency: -11&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 11:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996672#M147855</guid>
      <dc:creator>m_c</dc:creator>
      <dc:date>2019-11-01T11:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini cpufreq error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996673#M147856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi m.c.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;from log actually this is industrial i.MX8MMQL (max. operating frequency 1.6GHz),&lt;BR /&gt;so one can try to remove in dts:&lt;BR /&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8mm.dtsi?h=imx_4.14.98_2.2.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8mm.dtsi?h=imx_4.14.98_2.2.0"&gt;fsl-imx8mm.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&amp;amp;A53_0 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;operating-points = &amp;lt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* kHz&amp;nbsp;&amp;nbsp;&amp;nbsp; uV */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;1800000 1000000&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 23:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996673#M147856</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-11-01T23:29:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini cpufreq error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996674#M147857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have the same problem, but the point is our CPU is a commercial i.MX8MMD, which the U-boot log shows the max CPU-freq is 1.8GHz:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran a simple test during weekend and when I returned, faced this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The test which I ran during weekend was:&lt;/P&gt;&lt;P&gt;running a script, which executes the gpu-viv tutorials (/opt/viv_samples/vdk) one after each other and repeats the execution. After 3 days, I faced the below situation:&lt;/P&gt;&lt;P&gt;- black screen&lt;/P&gt;&lt;P&gt;- unreachable serial console&lt;/P&gt;&lt;P&gt;- continuously printing the below error on the serial console:&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;cpu cpu0: failed to scale arm_reg up: -11&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;cpufreq: __target_index: Failed to change cpu frequency: -11&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;This is the log of our U-boot. We also use the NXP-BSP with kernel 4.14.98&lt;/P&gt;&lt;P style="margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2018.03-00009-gfb8fa85 (Feb 05 2020 - 17:17:16 +0100)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MMD rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 50C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: FSL i.MX8MM EVK board&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage select!&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt; - ATF 1cb68fa&lt;BR /&gt; - U-Boot 2018.03-00009-gfb8fa85&lt;/P&gt;&lt;P&gt;Card did not respond to voltage select!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net: &lt;BR /&gt;Error: ethernet@30be0000 address not set.&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Reyhaneh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2020 16:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/996674#M147857</guid>
      <dc:creator>reyhanehyazdani</dc:creator>
      <dc:date>2020-02-05T16:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini cpufreq error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/1165933#M163299</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Igor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have the same problem, but the point is our CPU is a commercial&amp;nbsp;i.MX8MMQ rev1.0 1800 MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is the problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 08:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-cpufreq-error/m-p/1165933#M163299</guid>
      <dc:creator>wang_david-yb</dc:creator>
      <dc:date>2020-10-12T08:18:17Z</dc:date>
    </item>
  </channel>
</rss>