<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6sx ethernet issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6sx-ethernet-issue/m-p/1165640#M163267</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using two ethernet ports on our custom board imx6sx and using the yocto zeus kernel.&lt;/P&gt;&lt;P&gt;We figuring out at a time only one Ethernet port is working.&lt;/P&gt;&lt;P&gt;Also we observed when I start the ping from our board to PC directly it’s not started. It only start either we ping from PC to board or we can send some traffic through our PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help will be appriciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nikhil&lt;/P&gt;</description>
    <pubDate>Sun, 11 Oct 2020 10:21:47 GMT</pubDate>
    <dc:creator>nikhil_sahu2</dc:creator>
    <dc:date>2020-10-11T10:21:47Z</dc:date>
    <item>
      <title>IMX6sx ethernet issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6sx-ethernet-issue/m-p/1165640#M163267</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using two ethernet ports on our custom board imx6sx and using the yocto zeus kernel.&lt;/P&gt;&lt;P&gt;We figuring out at a time only one Ethernet port is working.&lt;/P&gt;&lt;P&gt;Also we observed when I start the ping from our board to PC directly it’s not started. It only start either we ping from PC to board or we can send some traffic through our PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help will be appriciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nikhil&lt;/P&gt;</description>
      <pubDate>Sun, 11 Oct 2020 10:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6sx-ethernet-issue/m-p/1165640#M163267</guid>
      <dc:creator>nikhil_sahu2</dc:creator>
      <dc:date>2020-10-11T10:21:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6sx ethernet issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6sx-ethernet-issue/m-p/1166668#M163394</link>
      <description>&lt;P&gt;First, please try to migrate to the latest L5.4.47_2.2.0 BSP, available here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If this does not help, I will raise a ticket to our SW team to fix the issue.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Artur&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 10:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6sx-ethernet-issue/m-p/1166668#M163394</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2020-10-13T10:33:33Z</dc:date>
    </item>
  </channel>
</rss>