<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MM based device stuck in recovery mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165440#M163251</link>
    <description>&lt;P&gt;Hi namanthaker&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if issue is observed only on one of the device, this may be hardware issue,&lt;/P&gt;
&lt;P&gt;for example poor soldering. One can try to resolder chip and check hardware&lt;/P&gt;
&lt;P&gt;using&amp;nbsp; &lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Sat, 10 Oct 2020 00:28:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-10-10T00:28:06Z</dc:date>
    <item>
      <title>IMX8MM based device stuck in recovery mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165149#M163206</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a custom device based on IMX8MM-EVK with Android 9 (p9.0.0_2.3.0) OS.&lt;BR /&gt;I have multiple devices, but one of the device is stuck in recovery mode. I need help to boot the device back into normal mode.&lt;/P&gt;&lt;P&gt;Steps performed on this device before it rebooted into recovery mode:&lt;BR /&gt;1. Start my custom application which starts the IMX8MM processor watchdog and kicks it at regular interval from a thread.&lt;BR /&gt;2. Uninstall the app while it was running.&lt;BR /&gt;3. Watchdog bite occurred as it was not kicked within required interval by the application.&lt;BR /&gt;4. Board rebooted into recovery mode.&lt;/P&gt;&lt;P&gt;Further information about the application and watchdog use-case:&lt;BR /&gt;In our devices, we have a feature to reboot the device in case the Android application stops working for some reason like app hang or crash.&lt;BR /&gt;The application starts the watchdog and kicks it at regular interval. In case the app stops working, the watchdog will reboot the device.&lt;BR /&gt;We are able to access the watchdog from application and when the app stops the device reboots in normal mode.&lt;BR /&gt;But this time for some reason, the device rebooted into recovery mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Steps performed to recover the device:&lt;BR /&gt;1. Reboot the device multiple times using below methods:&lt;BR /&gt;a. Perform power cycle by removing and then reconnecting power supply.&lt;BR /&gt;b. Power-off the device using ONOFF switch and then power it back on using the same switch.&lt;BR /&gt;&lt;BR /&gt;Both of the above methods worked on other devices which were put into recovery mode by running 'reboot recovery' command. But that does not happen on this one device.&lt;/P&gt;&lt;P&gt;2. Re-flash the BSP images using UUU tool after putting the device into Serial Download mode.&lt;BR /&gt;After flashing, the device booted in normal mode the first time. But then it stopped in the middle of booting and rebooted into recovery mode.&lt;/P&gt;&lt;P&gt;Refer attached normal_mode_bootup_logs.txt logs for the first time booting after flashing. The recovery_mode_bootup_logs.txt file contains logs observed while device boots into recovery mode.&lt;/P&gt;&lt;P&gt;Could someone please help to suggest some steps to recover the board from recovery mode?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 11:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165149#M163206</guid>
      <dc:creator>namanthaker</dc:creator>
      <dc:date>2020-10-09T11:32:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM based device stuck in recovery mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165440#M163251</link>
      <description>&lt;P&gt;Hi namanthaker&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if issue is observed only on one of the device, this may be hardware issue,&lt;/P&gt;
&lt;P&gt;for example poor soldering. One can try to resolder chip and check hardware&lt;/P&gt;
&lt;P&gt;using&amp;nbsp; &lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 10 Oct 2020 00:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165440#M163251</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-10-10T00:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM based device stuck in recovery mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165868#M163294</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;&lt;P&gt;We will try to resolder the chip, but first we would like to find the root cause of the issue on the device.&lt;/P&gt;&lt;P&gt;Could you suggest if there is any specific pin on IMX8MM processor which need to be set either high or low to start the processor in recovery mode?&lt;/P&gt;&lt;P&gt;We have observed on other processors that when a device is booted while pressing the power button along with Volume Up or Down key, the device will boot into recovery mode. Does IMX8MM support any such feature?&lt;BR /&gt;If yes, we would like to debug that pin and its connection first before we resolder the chip.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Naman&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 07:16:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1165868#M163294</guid>
      <dc:creator>namanthaker</dc:creator>
      <dc:date>2020-10-12T07:16:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM based device stuck in recovery mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1171550#M163871</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Igor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We were able to recover the device by flashing new images with Watchdog disabled in U-boot and erasing the User-data while flashing using '-e' option in uuu_imx_android_flash. The board is now booting properly in normal mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;BR /&gt;Naman&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 05:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-based-device-stuck-in-recovery-mode/m-p/1171550#M163871</guid>
      <dc:creator>namanthaker</dc:creator>
      <dc:date>2020-10-22T05:17:07Z</dc:date>
    </item>
  </channel>
</rss>