<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Compiling Kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-Kernel/m-p/1165089#M163199</link>
    <description>&lt;P&gt;I was using Android 7.1 with EDM1-iMX6 Dual Lite board with Fairy as baseboard.&lt;BR /&gt;On using flashcard script to flash the code boot partition was created with zImage in Android 7.1.&lt;BR /&gt;We would make changes to the kernel with &lt;EM&gt;&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt;&lt;/EM&gt; and fire the command &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; to update the build and the changes were reflected.&lt;BR /&gt;Now I am switching to Android 9.0 with EDM1-iMX6Q board with Fairy as baseboard.&lt;BR /&gt;On using the same script the partitions are different and there is no boot folder or I cannot see any &lt;EM&gt;&lt;STRONG&gt;zImage&lt;/STRONG&gt;&lt;/EM&gt; in the folder.&amp;nbsp;&lt;BR /&gt;I make changes to the kernel with &lt;EM&gt;&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt; &lt;/EM&gt;but &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; does not reflect the same.&lt;BR /&gt;What command do I use instead on &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; to update my changes from make menuconfig ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 09 Oct 2020 09:56:57 GMT</pubDate>
    <dc:creator>Ketki</dc:creator>
    <dc:date>2020-10-09T09:56:57Z</dc:date>
    <item>
      <title>Compiling Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-Kernel/m-p/1165089#M163199</link>
      <description>&lt;P&gt;I was using Android 7.1 with EDM1-iMX6 Dual Lite board with Fairy as baseboard.&lt;BR /&gt;On using flashcard script to flash the code boot partition was created with zImage in Android 7.1.&lt;BR /&gt;We would make changes to the kernel with &lt;EM&gt;&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt;&lt;/EM&gt; and fire the command &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; to update the build and the changes were reflected.&lt;BR /&gt;Now I am switching to Android 9.0 with EDM1-iMX6Q board with Fairy as baseboard.&lt;BR /&gt;On using the same script the partitions are different and there is no boot folder or I cannot see any &lt;EM&gt;&lt;STRONG&gt;zImage&lt;/STRONG&gt;&lt;/EM&gt; in the folder.&amp;nbsp;&lt;BR /&gt;I make changes to the kernel with &lt;EM&gt;&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt; &lt;/EM&gt;but &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; does not reflect the same.&lt;BR /&gt;What command do I use instead on &lt;EM&gt;&lt;STRONG&gt;make zImage&lt;/STRONG&gt;&lt;/EM&gt; to update my changes from make menuconfig ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 09:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiling-Kernel/m-p/1165089#M163199</guid>
      <dc:creator>Ketki</dc:creator>
      <dc:date>2020-10-09T09:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: Compiling Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-Kernel/m-p/1165253#M163225</link>
      <description>&lt;P&gt;Hello Ketki,&lt;/P&gt;
&lt;P&gt;Is possible that you run the script instead of kernel image then you have the virtual kernel partition overwrites only the kernel (zImage, zImage-dtb, Image.gz-dtb) by writing the new image.&lt;/P&gt;
&lt;P&gt;But you need the Zimage you have to&amp;nbsp;git clone&amp;nbsp;&lt;A class="link-bare" title="https://source.codeaurora.org/external/imx/linux-imx" href="https://source.codeaurora.org/external/imx/linux-imx" rel="nofollow noopener noreferrer" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx&lt;/A&gt; and menuconfig and make your configuration and build. &lt;/P&gt;
&lt;P&gt;You may ask&amp;nbsp; to EDM1-iMX6 manufacturer if they changed the script.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 13:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiling-Kernel/m-p/1165253#M163225</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-10-09T13:56:44Z</dc:date>
    </item>
  </channel>
</rss>