<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Is it necessary to configure USB ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1164532#M163122</link>
    <description>&lt;P&gt;Hello Okwaj,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using a dtb from Sabre board you don´t need because is there. but if you are on a custom board you have to take a look at the IOMUX that affects that USB, if there is none you don´t need it.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2020 13:03:47 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-10-08T13:03:47Z</dc:date>
    <item>
      <title>Is it necessary to configure USB ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1163985#M163057</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have 2 USB connected to my iMX6.&lt;/P&gt;&lt;P&gt;The first one is connected to CPU_USB2_D_N and&amp;nbsp;CPU_USB2_D_P pins.&lt;BR /&gt;The second one is connected to USB_OTG1_DN and USB_OTG1_DP.&lt;BR /&gt;&lt;BR /&gt;In the reference guide, it is said that the interface are natives.&lt;/P&gt;&lt;P&gt;Does it means that I have nothing to put inside the dtsi file to configure them ?&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 14:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1163985#M163057</guid>
      <dc:creator>okwaj</dc:creator>
      <dc:date>2020-10-07T14:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: Is it necessary to configure USB ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1164532#M163122</link>
      <description>&lt;P&gt;Hello Okwaj,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using a dtb from Sabre board you don´t need because is there. but if you are on a custom board you have to take a look at the IOMUX that affects that USB, if there is none you don´t need it.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 13:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1164532#M163122</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-10-08T13:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: Is it necessary to configure USB ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1166143#M163330</link>
      <description>&lt;P&gt;I am using a compulab imx6ul and it doesn't seem to work without configuration.&lt;/P&gt;&lt;P&gt;My 2 USB are plugged to pin 170/172 and 176/178 but I don't understand how to configure them in the dtsi file.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 14:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1166143#M163330</guid>
      <dc:creator>okwaj</dc:creator>
      <dc:date>2020-10-12T14:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is it necessary to configure USB ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1171825#M163899</link>
      <description>&lt;P&gt;Just had to do :&lt;/P&gt;&lt;P&gt;&amp;amp;usbotg1 {&lt;BR /&gt;dr_mode = "host";&lt;BR /&gt;disable-over-current;&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;amp;usbotg2 {&lt;BR /&gt;dr_mode = "host";&lt;BR /&gt;disable-over-current;&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 12:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-necessary-to-configure-USB/m-p/1171825#M163899</guid>
      <dc:creator>okwaj</dc:creator>
      <dc:date>2020-10-22T12:12:52Z</dc:date>
    </item>
  </channel>
</rss>