<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Minimal schematic for MIMXRT1062DVL6A?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Minimal-schematic-for-MIMXRT1062DVL6A/m-p/1164299#M163091</link>
    <description>&lt;P&gt;There is no dedicated "minimal" schematic available for the i.MX RT1062 processor. However, it can easily be defined.&lt;/P&gt;
&lt;P&gt;Please refer to the i.MX RT1062 EVK board schematic, available here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The minimum operating environment requires the power supply as shown on the Sheet 4 of the schematic above, at least one of possible boot media devices out of shown on the Sheet 11, boot configuration resistor network as shown on the Sheet 16 and the USB OTG port to program the device in the Serial Downloader mode as shown on the Sheet 7.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2020 05:13:26 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2020-10-08T05:13:26Z</dc:date>
    <item>
      <title>Minimal schematic for MIMXRT1062DVL6A?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Minimal-schematic-for-MIMXRT1062DVL6A/m-p/1162827#M162903</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;is there a minimal schematic for the&amp;nbsp;iMXRT1062 available somewhere? Means no perihperals, only these components that are required to start it successfully at full speed?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 09:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Minimal-schematic-for-MIMXRT1062DVL6A/m-p/1162827#M162903</guid>
      <dc:creator>Elmi77</dc:creator>
      <dc:date>2020-10-05T09:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: Minimal schematic for MIMXRT1062DVL6A?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Minimal-schematic-for-MIMXRT1062DVL6A/m-p/1164299#M163091</link>
      <description>&lt;P&gt;There is no dedicated "minimal" schematic available for the i.MX RT1062 processor. However, it can easily be defined.&lt;/P&gt;
&lt;P&gt;Please refer to the i.MX RT1062 EVK board schematic, available here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The minimum operating environment requires the power supply as shown on the Sheet 4 of the schematic above, at least one of possible boot media devices out of shown on the Sheet 11, boot configuration resistor network as shown on the Sheet 16 and the USB OTG port to program the device in the Serial Downloader mode as shown on the Sheet 7.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 05:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Minimal-schematic-for-MIMXRT1062DVL6A/m-p/1164299#M163091</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2020-10-08T05:13:26Z</dc:date>
    </item>
  </channel>
</rss>