<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux Image/Text Display Application using Yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Image-Text-Display-Application-using-Yocto/m-p/1163222#M162953</link>
    <description>&lt;DIV&gt;Hello everyone,&lt;/DIV&gt;&lt;DIV&gt;We are using the i.MX8QXP&amp;nbsp;MEK development board and we are developing Linux-based applications in Yocto.&lt;/DIV&gt;&lt;DIV&gt;We have connected the LVDS to the HDMI&amp;nbsp;converter (connected to LVDS0) to connect with the external display monitor.&lt;/DIV&gt;&lt;DIV&gt;We can load and boot, u-boot and Linux with rootfs from the emmc card. We can see the splash screen on the HD display in u-boot as well as Linux.&lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;We are trying to develop a user application to display the .jpeg/.jpg HD images(1080p) and user text (logs/ text files) on the HD display.&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;We are using the following components:&lt;/DIV&gt;&lt;UL&gt;&lt;LI&gt;Kernel version: L5.4.24_2.1.0&lt;/LI&gt;&lt;LI&gt;Image: core-image-base&lt;/LI&gt;&lt;LI&gt;Distro: x-Wayland&lt;/LI&gt;&lt;/UL&gt;&lt;DIV&gt;Please suggest a reference/way for developing an application with given components and hardware.&lt;BR /&gt;Thank&amp;nbsp;you&lt;/DIV&gt;</description>
    <pubDate>Wed, 07 Oct 2020 13:30:51 GMT</pubDate>
    <dc:creator>barish_malshika</dc:creator>
    <dc:date>2020-10-07T13:30:51Z</dc:date>
    <item>
      <title>Linux Image/Text Display Application using Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Image-Text-Display-Application-using-Yocto/m-p/1163222#M162953</link>
      <description>&lt;DIV&gt;Hello everyone,&lt;/DIV&gt;&lt;DIV&gt;We are using the i.MX8QXP&amp;nbsp;MEK development board and we are developing Linux-based applications in Yocto.&lt;/DIV&gt;&lt;DIV&gt;We have connected the LVDS to the HDMI&amp;nbsp;converter (connected to LVDS0) to connect with the external display monitor.&lt;/DIV&gt;&lt;DIV&gt;We can load and boot, u-boot and Linux with rootfs from the emmc card. We can see the splash screen on the HD display in u-boot as well as Linux.&lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;We are trying to develop a user application to display the .jpeg/.jpg HD images(1080p) and user text (logs/ text files) on the HD display.&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;We are using the following components:&lt;/DIV&gt;&lt;UL&gt;&lt;LI&gt;Kernel version: L5.4.24_2.1.0&lt;/LI&gt;&lt;LI&gt;Image: core-image-base&lt;/LI&gt;&lt;LI&gt;Distro: x-Wayland&lt;/LI&gt;&lt;/UL&gt;&lt;DIV&gt;Please suggest a reference/way for developing an application with given components and hardware.&lt;BR /&gt;Thank&amp;nbsp;you&lt;/DIV&gt;</description>
      <pubDate>Wed, 07 Oct 2020 13:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Image-Text-Display-Application-using-Yocto/m-p/1163222#M162953</guid>
      <dc:creator>barish_malshika</dc:creator>
      <dc:date>2020-10-07T13:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Image/Text Display Application using Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Image-Text-Display-Application-using-Yocto/m-p/1164385#M163103</link>
      <description>&lt;P&gt;Your question seems not to be specific to any of the NXP products, but to be a kind of general Linux development question.&lt;/P&gt;
&lt;P&gt;So, first, please refer to generally available Linux developer resources.&lt;/P&gt;
&lt;P&gt;Some general Linux development related Application Note documents are available from NXP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3870.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN3870.pdf&lt;/A&gt; &lt;A href="https://www.nxp.com/docs/en/application-note/AN4553.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf &lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, please refer to the documentation, specific to the Linux BSP you use.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Artur&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 08:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Image-Text-Display-Application-using-Yocto/m-p/1164385#M163103</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2020-10-08T08:38:39Z</dc:date>
    </item>
  </channel>
</rss>