<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.Mx8MQ u-boot boot up issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx8MQ-u-boot-boot-up-issue/m-p/1163000#M162922</link>
    <description>&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Hi NXP Team,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;We have used imx8mq_evk for development purposes. Based on the imx8mq evk design we have developed a custom board.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Flash process:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the processes which we have followed:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;1. I have refer to the DDR calibration tool and doing a DDR stress test.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;2. After the stress test successfully,&amp;nbsp; I have generated lpddr.c file.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;3. After generating lpddr.c stress file I have integrated this file into the u-boot.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;4. Compile the u-boot and flash the u-boot using uuu tool.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Boot process:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the processes which we have followed After flashing the images:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT face="verdana,geneva"&gt;I changed the boot pin setting and set it as an internal boot mode&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Boot process observation:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the logs which I have received in the UART console at boot-up time.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;###################################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;U-Boot 2019.04-lf-5.4.y_v2019.04+g08ae210 (Oct 05 2020 - 14:24:44 +0000)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;CPU: Freescale i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;CPU: Commercial temperature grade (0C to 95C) at 33C&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Reset cause: POR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Model: i.MX8MQ&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;DRAM: 4 GiB&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Loading Environment from MMC... MMC: no card present&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;*** Warning - No block device, using default environment&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;In: serial&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Out: serial&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Err: serial&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;BuildInfo:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;- ATF 7b3389d&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;- U-Boot 2019.04-lf-5.4.y_v2019.04+g08ae210&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;MMC: no card present&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Detect USB boot. Will enter fastboot mode!&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Net:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Error: ethernet@30be0000 address not set.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Error: ethernet@30be0000 address not set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;eth-1: ethernet@30be0000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Fastboot: Normal&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Boot from USB for mfgtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;*** Warning - Use default environment for mfgtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;, using default environment&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; f&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;i;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Hit any key to stop autoboot: 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt; U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 201&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;9.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT face="verdana,geneva"&gt;Questions:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT face="verdana,geneva"&gt;&lt;STRONG&gt;Why u-boot stuck after reaching command prompt?&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Mon, 05 Oct 2020 15:13:34 GMT</pubDate>
    <dc:creator>neel_desai</dc:creator>
    <dc:date>2020-10-05T15:13:34Z</dc:date>
    <item>
      <title>i.Mx8MQ u-boot boot up issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx8MQ-u-boot-boot-up-issue/m-p/1163000#M162922</link>
      <description>&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Hi NXP Team,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;We have used imx8mq_evk for development purposes. Based on the imx8mq evk design we have developed a custom board.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Flash process:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the processes which we have followed:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;1. I have refer to the DDR calibration tool and doing a DDR stress test.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;2. After the stress test successfully,&amp;nbsp; I have generated lpddr.c file.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;3. After generating lpddr.c stress file I have integrated this file into the u-boot.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;4. Compile the u-boot and flash the u-boot using uuu tool.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Boot process:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the processes which we have followed After flashing the images:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT face="verdana,geneva"&gt;I changed the boot pin setting and set it as an internal boot mode&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;&lt;U&gt;&lt;STRONG&gt;Boot process observation:&lt;/STRONG&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Below are the logs which I have received in the UART console at boot-up time.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;###################################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;U-Boot 2019.04-lf-5.4.y_v2019.04+g08ae210 (Oct 05 2020 - 14:24:44 +0000)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;CPU: Freescale i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;CPU: Commercial temperature grade (0C to 95C) at 33C&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Reset cause: POR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Model: i.MX8MQ&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;DRAM: 4 GiB&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Loading Environment from MMC... MMC: no card present&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;*** Warning - No block device, using default environment&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;In: serial&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Out: serial&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Err: serial&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;BuildInfo:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;- ATF 7b3389d&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;- U-Boot 2019.04-lf-5.4.y_v2019.04+g08ae210&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;MMC: no card present&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Detect USB boot. Will enter fastboot mode!&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Net:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Error: ethernet@30be0000 address not set.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Error: ethernet@30be0000 address not set.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;eth-1: ethernet@30be0000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Fastboot: Normal&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Boot from USB for mfgtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;*** Warning - Use default environment for mfgtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;, using default environment&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="verdana,geneva"&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; f&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;i;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;Hit any key to stop autoboot: 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;u-boot=&amp;gt; U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 201&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;9.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="verdana,geneva"&gt;.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U-Boot 2019.04-lf-5.4.y_v201 U&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT face="verdana,geneva"&gt;Questions:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT face="verdana,geneva"&gt;&lt;STRONG&gt;Why u-boot stuck after reaching command prompt?&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Mon, 05 Oct 2020 15:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx8MQ-u-boot-boot-up-issue/m-p/1163000#M162922</guid>
      <dc:creator>neel_desai</dc:creator>
      <dc:date>2020-10-05T15:13:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx8MQ u-boot boot up issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx8MQ-u-boot-boot-up-issue/m-p/1165444#M163252</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I see no errors in the log you had shared, is the boot log I presume, the only thing that I could say about this is that you had stopped at uboot.&lt;BR /&gt;&lt;BR /&gt;Does it not start kernel automatically if you let the countdown finish?&lt;BR /&gt;Once uboot start do not input any character to the serial terminal since this will stop uboot as you can see in your test.&lt;BR /&gt;&lt;BR /&gt;Hope this helps,&lt;BR /&gt;Regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 10 Oct 2020 00:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx8MQ-u-boot-boot-up-issue/m-p/1165444#M163252</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2020-10-10T00:50:57Z</dc:date>
    </item>
  </channel>
</rss>