<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q6AVT10AC Decoder And Encoder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q6AVT10AC-Decoder-And-Encoder/m-p/226834#M16277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please take a look to the community thread,&lt;A href="https://community.nxp.com/thread/307038"&gt;Memory Reserved on i.MX6 for VPU&lt;/A&gt;.&amp;nbsp; Increasing the clock it is not going to be the solution,&amp;nbsp; I think you are getting a bottleneck in the memory allocation of the VPU which it is in charge of making the decoding and encoding, so if you provide more memory you can get a better performance of the device.&amp;nbsp; Or you can try as a test decrease the framerate, so the VPU needs less memory to work and would be able to handle faster.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jan 2014 20:46:43 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2014-01-21T20:46:43Z</dc:date>
    <item>
      <title>IMX6Q6AVT10AC Decoder And Encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q6AVT10AC-Decoder-And-Encoder/m-p/226833#M16276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,everybody&lt;/P&gt;&lt;P&gt;I have a test the performance of the I.MX6Q(1.0G) decoder and encoder.&lt;/P&gt;&lt;P&gt;I decode a file of 1080P30fps use H.264 standard. After decoder finish decode, sent the buffer to display and encoder.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;At last,when the Ecoder finish ,it save buffer to a H.264 standard video file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I find it cost about 43ms to decode and encode.When I do not sent the buffer to display, it cost about 37ms.&lt;/P&gt;&lt;P&gt;1080p30fps video&amp;nbsp; only have 33ms between two frame.&lt;/P&gt;&lt;P&gt;How can I improve I.MX6 decoder and encoder performance?Using a 1.2G CPU or&amp;nbsp; can I increase VPU clock to do it?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 02:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q6AVT10AC-Decoder-And-Encoder/m-p/226833#M16276</guid>
      <dc:creator>carmilili</dc:creator>
      <dc:date>2014-01-10T02:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q6AVT10AC Decoder And Encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q6AVT10AC-Decoder-And-Encoder/m-p/226834#M16277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please take a look to the community thread,&lt;A href="https://community.nxp.com/thread/307038"&gt;Memory Reserved on i.MX6 for VPU&lt;/A&gt;.&amp;nbsp; Increasing the clock it is not going to be the solution,&amp;nbsp; I think you are getting a bottleneck in the memory allocation of the VPU which it is in charge of making the decoding and encoding, so if you provide more memory you can get a better performance of the device.&amp;nbsp; Or you can try as a test decrease the framerate, so the VPU needs less memory to work and would be able to handle faster.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 20:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q6AVT10AC-Decoder-And-Encoder/m-p/226834#M16277</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-01-21T20:46:43Z</dc:date>
    </item>
  </channel>
</rss>