<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6Q Yocto project fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Yocto-project-fail/m-p/1161452#M162765</link>
    <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P&gt;I configure the yocto project as shown in Figure 1 ,&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git" target="_blank"&gt;https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git&lt;/A&gt; -b imx-morty -m imx-4.9.11-1.0.0_ga.xml&lt;/P&gt;&lt;P&gt;repo sync&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;/P&gt;&lt;P&gt;bitbake fsl-image-qt5-validation-imx&lt;/P&gt;&lt;P&gt;The error is shown in Figure 2&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 17:04:48 GMT</pubDate>
    <dc:creator>dt_liumi</dc:creator>
    <dc:date>2020-09-30T17:04:48Z</dc:date>
    <item>
      <title>IMX6Q Yocto project fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Yocto-project-fail/m-p/1161452#M162765</link>
      <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P&gt;I configure the yocto project as shown in Figure 1 ,&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git" target="_blank"&gt;https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git&lt;/A&gt; -b imx-morty -m imx-4.9.11-1.0.0_ga.xml&lt;/P&gt;&lt;P&gt;repo sync&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;/P&gt;&lt;P&gt;bitbake fsl-image-qt5-validation-imx&lt;/P&gt;&lt;P&gt;The error is shown in Figure 2&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 17:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Yocto-project-fail/m-p/1161452#M162765</guid>
      <dc:creator>dt_liumi</dc:creator>
      <dc:date>2020-09-30T17:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q Yocto project fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Yocto-project-fail/m-p/1161839#M162814</link>
      <description>&lt;P&gt;Hello dt_liumi,&lt;/P&gt;
&lt;P&gt;You can download another BSP, because the L4.9.11 is out of support since it tries to download the firmware from freescale,com and that´s the fails. you can download the BSP from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Oct 2020 13:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Yocto-project-fail/m-p/1161839#M162814</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-10-01T13:14:25Z</dc:date>
    </item>
  </channel>
</rss>