<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックProblems with HAB and MFG tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-HAB-and-MFG-tool/m-p/1159594#M162580</link>
    <description>&lt;P&gt;I am enabling secure boot in i.MX6 ULL platform, i am getting HAB events while flashing from MFG tool.&lt;/P&gt;&lt;P&gt;&amp;lt;mfg firmware zImage&amp;gt; while loading this HAB events are comming.&lt;/P&gt;&lt;P&gt;There is no hab events after booting the board.&lt;/P&gt;&lt;P&gt;I have not closed the board yet.&lt;/P&gt;&lt;P&gt;Please help me in fixing this HAB events issue with MFG tool.&lt;/P&gt;&lt;P&gt;U-Boot 2015.04 (Sep 25 2020 - 14:15:05)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX?? rev1.1 at 396 MHz&lt;BR /&gt;CPU: Temperature 42 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: i.MX6UL&lt;BR /&gt;Boot Device: MMC2&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current devic&lt;/P&gt;&lt;P&gt;Net: FEC1&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x5c6010 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 8591032 Bytes = 8.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x80800000...&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x33 0x18 0xc0 0x00&lt;BR /&gt;0xca 0x00 0x1c 0x00 0x00 0xc5 0xff 0x00&lt;BR /&gt;0x00 0x00 0x09 0xc8 0x87 0x7f 0xf4 0x00&lt;BR /&gt;0x00 0x04 0x7c 0x00 0x00 0x91 0x00 0x00&lt;BR /&gt;0x00 0x00 0x01 0xf0&lt;/P&gt;&lt;P&gt;--------- HAB Event 2 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00&lt;BR /&gt;0x00 0x00 0x00 0x20&lt;/P&gt;&lt;P&gt;--------- HAB Event 3 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;--------- HAB Event 4 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x04&lt;/P&gt;&lt;P&gt;--------- HAB Event 5 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00&lt;BR /&gt;0x00 0x00 0x01 0xe8&lt;BR /&gt;Using Device Tree in place at 83000000, end 83009619&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 26 Sep 2020 14:52:19 GMT</pubDate>
    <dc:creator>shashikanthacha</dc:creator>
    <dc:date>2020-09-26T14:52:19Z</dc:date>
    <item>
      <title>Problems with HAB and MFG tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-HAB-and-MFG-tool/m-p/1159594#M162580</link>
      <description>&lt;P&gt;I am enabling secure boot in i.MX6 ULL platform, i am getting HAB events while flashing from MFG tool.&lt;/P&gt;&lt;P&gt;&amp;lt;mfg firmware zImage&amp;gt; while loading this HAB events are comming.&lt;/P&gt;&lt;P&gt;There is no hab events after booting the board.&lt;/P&gt;&lt;P&gt;I have not closed the board yet.&lt;/P&gt;&lt;P&gt;Please help me in fixing this HAB events issue with MFG tool.&lt;/P&gt;&lt;P&gt;U-Boot 2015.04 (Sep 25 2020 - 14:15:05)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX?? rev1.1 at 396 MHz&lt;BR /&gt;CPU: Temperature 42 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: i.MX6UL&lt;BR /&gt;Boot Device: MMC2&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current devic&lt;/P&gt;&lt;P&gt;Net: FEC1&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x5c6010 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 8591032 Bytes = 8.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x80800000...&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x33 0x18 0xc0 0x00&lt;BR /&gt;0xca 0x00 0x1c 0x00 0x00 0xc5 0xff 0x00&lt;BR /&gt;0x00 0x00 0x09 0xc8 0x87 0x7f 0xf4 0x00&lt;BR /&gt;0x00 0x04 0x7c 0x00 0x00 0x91 0x00 0x00&lt;BR /&gt;0x00 0x00 0x01 0xf0&lt;/P&gt;&lt;P&gt;--------- HAB Event 2 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00&lt;BR /&gt;0x00 0x00 0x00 0x20&lt;/P&gt;&lt;P&gt;--------- HAB Event 3 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;--------- HAB Event 4 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x04&lt;/P&gt;&lt;P&gt;--------- HAB Event 5 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00&lt;BR /&gt;0x00 0x00 0x01 0xe8&lt;BR /&gt;Using Device Tree in place at 83000000, end 83009619&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 26 Sep 2020 14:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-HAB-and-MFG-tool/m-p/1159594#M162580</guid>
      <dc:creator>shashikanthacha</dc:creator>
      <dc:date>2020-09-26T14:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with HAB and MFG tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-HAB-and-MFG-tool/m-p/1159779#M162599</link>
      <description>&lt;P&gt;Hi shashikanthacha&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can refer to below discussion,&lt;/P&gt;
&lt;P&gt;please pay attention to advice for Appendix E (Freescale manufacturing tool) of app note AN4581&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX6-HAB-secure-boot-fuse-problem/m-p/489919" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX6-HAB-secure-boot-fuse-problem/m-p/489919&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2020 01:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-HAB-and-MFG-tool/m-p/1159779#M162599</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-28T01:21:04Z</dc:date>
    </item>
  </channel>
</rss>