<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX 8 custom build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8-custom-build/m-p/1159582#M162579</link>
    <description>&lt;P&gt;Hello, I am trying to port the kernel "imx8mini" for the custom board. Following the manual&amp;nbsp; iMX Youcto Users Guide I created a "build" directory for MACHINE= imx8mmevk, DISTRO=fslc-wayland, with the command:&lt;/P&gt;&lt;P&gt;"MACHINE=imx8mmevk DISTRO=fslc-wayland source setup-environment build"&lt;/P&gt;&lt;P&gt;After that,&amp;nbsp; followed by manual "i.MX Reference Manual (chapter Porting Kernel )", I used the command:&lt;/P&gt;&lt;P&gt;DISTRO=fslc-wayland MACHINE=imx8mmevk bitbake core-image-minimal -c populate_sdk&lt;/P&gt;&lt;P&gt;And got the next error:&lt;/P&gt;&lt;P&gt;Loading cache: 100% |############################################| Time: 0:00:00&lt;BR /&gt;Loaded 1926 entries from dependency cache.&lt;BR /&gt;ERROR: ParseError at /home/sergey/Documents/nxp_proj/Yocto/sources/meta-freescale/recipes-multimedia/imx-codec/imx-codec_4.4.5.bb:17: Could not inherit file classes/fsl-eula-unpack.bbclass&lt;/P&gt;</description>
    <pubDate>Sat, 26 Sep 2020 11:25:49 GMT</pubDate>
    <dc:creator>SergeySm1</dc:creator>
    <dc:date>2020-09-26T11:25:49Z</dc:date>
    <item>
      <title>iMX 8 custom build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8-custom-build/m-p/1159582#M162579</link>
      <description>&lt;P&gt;Hello, I am trying to port the kernel "imx8mini" for the custom board. Following the manual&amp;nbsp; iMX Youcto Users Guide I created a "build" directory for MACHINE= imx8mmevk, DISTRO=fslc-wayland, with the command:&lt;/P&gt;&lt;P&gt;"MACHINE=imx8mmevk DISTRO=fslc-wayland source setup-environment build"&lt;/P&gt;&lt;P&gt;After that,&amp;nbsp; followed by manual "i.MX Reference Manual (chapter Porting Kernel )", I used the command:&lt;/P&gt;&lt;P&gt;DISTRO=fslc-wayland MACHINE=imx8mmevk bitbake core-image-minimal -c populate_sdk&lt;/P&gt;&lt;P&gt;And got the next error:&lt;/P&gt;&lt;P&gt;Loading cache: 100% |############################################| Time: 0:00:00&lt;BR /&gt;Loaded 1926 entries from dependency cache.&lt;BR /&gt;ERROR: ParseError at /home/sergey/Documents/nxp_proj/Yocto/sources/meta-freescale/recipes-multimedia/imx-codec/imx-codec_4.4.5.bb:17: Could not inherit file classes/fsl-eula-unpack.bbclass&lt;/P&gt;</description>
      <pubDate>Sat, 26 Sep 2020 11:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8-custom-build/m-p/1159582#M162579</guid>
      <dc:creator>SergeySm1</dc:creator>
      <dc:date>2020-09-26T11:25:49Z</dc:date>
    </item>
  </channel>
</rss>