<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adding an external platform library to AOSP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1156898#M162301</link>
    <description>&lt;DIV class="s-prose js-post-body"&gt;&lt;P&gt;I'm trying to add an external library to my AOSP (v9.0.0-2.0.0) image by following the instructions provided with said library. The instructions are:&lt;/P&gt;&lt;P&gt;cd &amp;lt;aosp source folder&amp;gt;/external/libgpiod&lt;/P&gt;&lt;P&gt;mm&lt;/P&gt;&lt;P&gt;Then I run luch and then make to build the image then I flashed it to the SD card. But when I the library commands it via adb shell, none of them work. Although I can see that there are some files name the same as the library in the /out folder.&lt;/P&gt;&lt;P&gt;Is there any way to debug this? The log file isn't helping me very much.&lt;/P&gt;&lt;P&gt;The library in question is &lt;A href="https://github.com/technexion-android/platform_external_libgpiod" target="_blank" rel="nofollow noopener noreferrer"&gt;https://github.com/technexion-android/platform_external_libgpiod&lt;/A&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class="post-taglist grid gs4 gsy fd-column"&gt;&lt;DIV class="grid ps-relative d-block"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 22 Sep 2020 11:55:08 GMT</pubDate>
    <dc:creator>imoya</dc:creator>
    <dc:date>2020-09-22T11:55:08Z</dc:date>
    <item>
      <title>Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1156898#M162301</link>
      <description>&lt;DIV class="s-prose js-post-body"&gt;&lt;P&gt;I'm trying to add an external library to my AOSP (v9.0.0-2.0.0) image by following the instructions provided with said library. The instructions are:&lt;/P&gt;&lt;P&gt;cd &amp;lt;aosp source folder&amp;gt;/external/libgpiod&lt;/P&gt;&lt;P&gt;mm&lt;/P&gt;&lt;P&gt;Then I run luch and then make to build the image then I flashed it to the SD card. But when I the library commands it via adb shell, none of them work. Although I can see that there are some files name the same as the library in the /out folder.&lt;/P&gt;&lt;P&gt;Is there any way to debug this? The log file isn't helping me very much.&lt;/P&gt;&lt;P&gt;The library in question is &lt;A href="https://github.com/technexion-android/platform_external_libgpiod" target="_blank" rel="nofollow noopener noreferrer"&gt;https://github.com/technexion-android/platform_external_libgpiod&lt;/A&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class="post-taglist grid gs4 gsy fd-column"&gt;&lt;DIV class="grid ps-relative d-block"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 22 Sep 2020 11:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1156898#M162301</guid>
      <dc:creator>imoya</dc:creator>
      <dc:date>2020-09-22T11:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157125#M162324</link>
      <description>&lt;P&gt;Que tal &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178276"&gt;@imoya&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;You do not need to add this library, it is already in the Android BSP of the board that you have, it is not necessary,&amp;nbsp; If you add a new library then need to be reported to the Android System, besides the Linux Kernel of the system.&amp;nbsp; some&amp;nbsp; kind of security features.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 18:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157125#M162324</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2020-09-22T18:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157711#M162377</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/10885"&gt;@jamesbone&lt;/a&gt;thanks for your feedback. I think there is something I am not understanding from this library.&lt;/P&gt;&lt;P&gt;When I try anyone of the shell commands none of them work. I get this output:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;dart_mx8mm:/ # gpiodetect&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;/system/bin/sh: gpiodetect: not found&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;And its the same for the rest of them, &lt;EM&gt;gpioinfo, gpioget, gpioset, gpiofind&lt;/EM&gt; and &lt;EM&gt;gpiomon. &lt;/EM&gt;If it is already installed, shouldn't they work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 11:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157711#M162377</guid>
      <dc:creator>imoya</dc:creator>
      <dc:date>2020-09-23T11:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157856#M162394</link>
      <description>&lt;P&gt;I think you need to contact Varicite, the board Manufacturer, in order to understand if the BSP has something else in the Kernel or in the rc file,&amp;nbsp; that need to be configure to use in the command shell the library.&lt;/P&gt;&lt;P&gt;Have you try to use it in an APK or in a program?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 15:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157856#M162394</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2020-09-23T15:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157894#M162397</link>
      <description>&lt;P&gt;Yes, I'm already in touch with them, but because of holidays in Israel I haven't got a reply yet.&lt;/P&gt;&lt;P&gt;I'm doing as you advised right know. I will post my results here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 16:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1157894#M162397</guid>
      <dc:creator>imoya</dc:creator>
      <dc:date>2020-09-23T16:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an external platform library to AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1161282#M162750</link>
      <description>&lt;P&gt;Thank you James,&lt;/P&gt;&lt;P&gt;yes the library was already included but that wasn't the case for the command-line tools of libgpiod, that was the reason why the commands didn't work.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 11:12:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-an-external-platform-library-to-AOSP/m-p/1161282#M162750</guid>
      <dc:creator>imoya</dc:creator>
      <dc:date>2020-09-30T11:12:59Z</dc:date>
    </item>
  </channel>
</rss>