<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Optimize linux boot up time on imx8mqevk</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156629#M162245</link>
    <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Fast-Boot-on-i-MX6-Sabresd-Board/ta-p/1102298" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Fast-Boot-on-i-MX6-Sabresd-Board/ta-p/1102298&lt;/A&gt; This is for i.mx6 series, you can refer to the method. Hope can do help for you.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Sep 2020 03:36:07 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2020-09-22T03:36:07Z</dc:date>
    <item>
      <title>Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1155304#M162074</link>
      <description>&lt;P&gt;How to optimize the linux boot up time on imx8mqevk and what are the required files to boot linux on mx8mqevk board&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 06:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1155304#M162074</guid>
      <dc:creator>Chandu</dc:creator>
      <dc:date>2020-09-18T06:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156619#M162241</link>
      <description>&lt;P&gt;Which version BSP are you using? Have your board already boot up?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 03:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156619#M162241</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-09-22T03:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156625#M162244</link>
      <description>&lt;P&gt;&lt;FONT style="font-family: Arial;"&gt;I can provide you some common recommendations.&lt;BR /&gt;You need to remove all unnecessary services from startup.&lt;BR /&gt;Also you can remove all unnecessary options and modules from the kernel.For example if you do not need ethernet you can compile the kernel without its support.&lt;BR /&gt;And also you can set maximum frequency. Later you can decrease frequency if you not need more performance.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 03:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156625#M162244</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-09-22T03:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156629#M162245</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Fast-Boot-on-i-MX6-Sabresd-Board/ta-p/1102298" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Fast-Boot-on-i-MX6-Sabresd-Board/ta-p/1102298&lt;/A&gt; This is for i.mx6 series, you can refer to the method. Hope can do help for you.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 03:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156629#M162245</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-09-22T03:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156883#M162296</link>
      <description>&lt;P&gt;Yes we already boot up the board. But we want to reduce the linux boot up time while booting on the imx8mqevk board. We are using imx-4.14.98-2.0.0 version and the branch is imx-linux-sumo.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 10:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156883#M162296</guid>
      <dc:creator>Chandu</dc:creator>
      <dc:date>2020-09-22T10:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: Optimize linux boot up time on imx8mqevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156884#M162297</link>
      <description>&lt;P&gt;Thank you but IMX6 series is different and imx8mqevk is different. We want to optimize Linux boot up time on imx8mqevk board and I want to remove unnecessary files. So, can you please send the steps to optimize Linux boot up time on imx8mqevk board.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 11:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Optimize-linux-boot-up-time-on-imx8mqevk/m-p/1156884#M162297</guid>
      <dc:creator>Chandu</dc:creator>
      <dc:date>2020-09-22T11:04:30Z</dc:date>
    </item>
  </channel>
</rss>