<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: bitbake meta-toolchain errors in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/1156440#M162219</link>
    <description>&lt;P&gt;I have same problem with build&amp;nbsp;QorIQ-SDK-V2.0-20160527-yocto (QorIQ-SDK-V2.0-1703)&lt;/P&gt;&lt;P&gt;I install&amp;nbsp;&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-SOURCE.iso&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-AARCH64-Yocto-Cache&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-1703.tar.bz2&lt;/P&gt;&lt;P&gt;follow the instruction,&lt;/P&gt;&lt;P&gt;run&amp;nbsp;./sources/meta-freescale/scripts/host-prepare.sh&amp;nbsp;&lt;/P&gt;&lt;P&gt;But i got error&lt;/P&gt;&lt;P&gt;| make[1]: Leaving directory '/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/build_ls1012afrdm/tmp/work/x86_64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.x86_64-linux.aarch64-fsl-linux/gcc'&lt;BR /&gt;| Makefile:3976: recipe for target 'all-gcc' failed&lt;BR /&gt;| make: *** [all-gcc] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/andrii/QorIQ-SDK-V2.0-20160527-yocto/build_ls1012afrdm/tmp/work/x86_64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/temp/log.do_compile.16433)&lt;BR /&gt;ERROR: Task 432 (/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/gcc/gcc-cross_linaro-4.9.bb, do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 505 tasks of which 413 didn't need to be rerun and 2 failed.&lt;/P&gt;&lt;P&gt;Summary: 2 tasks failed:&lt;BR /&gt;virtual:native:/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/poky/meta/recipes-devtools/prelink/prelink_git.bb, do_configure&lt;BR /&gt;/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/gcc/gcc-cross_linaro-4.9.bb, do_compile&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 3 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;I tried&amp;nbsp; build minimal image for&amp;nbsp;ls1012afrdm&lt;/P&gt;&lt;P&gt;bitbake fsl-image-minimal&lt;/P&gt;&lt;P&gt;What i"ll have to do else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2020 17:51:01 GMT</pubDate>
    <dc:creator>akrestov</dc:creator>
    <dc:date>2020-09-21T17:51:01Z</dc:date>
    <item>
      <title>bitbake meta-toolchain errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/392785#M57326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In trying to bake a toolchain (bitbake meta-toolchain) I get errors:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| Makefile:3976: recipe for target 'all-gcc' failed&lt;/P&gt;&lt;P&gt;| make: *** [all-gcc] Error 2&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_compile (log file is located at /home/osboxes/poky/build/tmp/work/x86_64-poky-linux/gcc-cross-aarch64/4.9.3-r0/temp/log.do_compile.2070)&lt;/P&gt;&lt;P&gt;ERROR: Task 107 (/home/osboxes/poky/meta/recipes-devtools/gcc/gcc-cross_4.9.bb, do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;Currently 3 running tasks (1059 of 2130):&lt;/P&gt;&lt;P&gt;0: gcc-crosssdk-x86_64-4.9.3-r0 do_compile (pid 2069)&lt;/P&gt;&lt;P&gt;1: glibc-locale-2.21-r0 do_package_qa (pid 2562)&lt;/P&gt;&lt;P&gt;2: glibc-locale-2.21-r0 do_package_write_rpm (pid 2565)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did anybody fall on this kind of error?&lt;/P&gt;&lt;P&gt;Appreciate your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best, Ioan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 16:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/392785#M57326</guid>
      <dc:creator>ioancalapod</dc:creator>
      <dc:date>2015-08-24T16:15:44Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake meta-toolchain errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/392786#M57327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ioan Calapod,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Would you please share the BSP you are using? Either the Freescale Community BSP or Freescale BSP Release and which branch/version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;It seems that the problem might be related with the setting up of the environment, would you please share the steps you’re following for specifying the Machine/Board you’re using?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 21:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/392786#M57327</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-08-26T21:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake meta-toolchain errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/1156440#M162219</link>
      <description>&lt;P&gt;I have same problem with build&amp;nbsp;QorIQ-SDK-V2.0-20160527-yocto (QorIQ-SDK-V2.0-1703)&lt;/P&gt;&lt;P&gt;I install&amp;nbsp;&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-SOURCE.iso&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-AARCH64-Yocto-Cache&lt;/P&gt;&lt;P&gt;QorIQ-Linux-SDK-v2.0-1703.tar.bz2&lt;/P&gt;&lt;P&gt;follow the instruction,&lt;/P&gt;&lt;P&gt;run&amp;nbsp;./sources/meta-freescale/scripts/host-prepare.sh&amp;nbsp;&lt;/P&gt;&lt;P&gt;But i got error&lt;/P&gt;&lt;P&gt;| make[1]: Leaving directory '/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/build_ls1012afrdm/tmp/work/x86_64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.x86_64-linux.aarch64-fsl-linux/gcc'&lt;BR /&gt;| Makefile:3976: recipe for target 'all-gcc' failed&lt;BR /&gt;| make: *** [all-gcc] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/andrii/QorIQ-SDK-V2.0-20160527-yocto/build_ls1012afrdm/tmp/work/x86_64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/temp/log.do_compile.16433)&lt;BR /&gt;ERROR: Task 432 (/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/gcc/gcc-cross_linaro-4.9.bb, do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 505 tasks of which 413 didn't need to be rerun and 2 failed.&lt;/P&gt;&lt;P&gt;Summary: 2 tasks failed:&lt;BR /&gt;virtual:native:/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/poky/meta/recipes-devtools/prelink/prelink_git.bb, do_configure&lt;BR /&gt;/home/andrii/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/gcc/gcc-cross_linaro-4.9.bb, do_compile&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 3 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;I tried&amp;nbsp; build minimal image for&amp;nbsp;ls1012afrdm&lt;/P&gt;&lt;P&gt;bitbake fsl-image-minimal&lt;/P&gt;&lt;P&gt;What i"ll have to do else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 17:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-meta-toolchain-errors/m-p/1156440#M162219</guid>
      <dc:creator>akrestov</dc:creator>
      <dc:date>2020-09-21T17:51:01Z</dc:date>
    </item>
  </channel>
</rss>